This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-cog-ad3029:software:aducm302x [10 Jul 2017 08:23] – Pranit Jadhav | resources:eval:user-guides:eval-cog-ad3029:software:aducm302x [12 Aug 2017 07:55] (current) – Pranit Jadhav | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADuCM302x On-Chip Peripheral Drivers & Software ====== | ====== ADuCM302x On-Chip Peripheral Drivers & Software ====== | ||
+ | ===== General Description/ | ||
+ | The ADuCM302x Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for both the [[ADI> | ||
+ | |||
+ | The following on-chip drivers are provided as part of the ADuCM302x Device Family Pack: | ||
+ | * spi{{ : | ||
+ | * i2c | ||
+ | * uart | ||
+ | * sport | ||
+ | * beep | ||
+ | * wdt | ||
+ | * gpio | ||
+ | * rtc | ||
+ | * dma | ||
+ | * cryto | ||
+ | * adc | ||
+ | * tmr | ||
+ | |||
+ | For detailed information regarding the ADuCM302x DFP, please see our complete ADuCM302x software user guide. | ||
+ | <WRAP center round help 60%> | ||
+ | |||
+ | | ||
+ | |||
+ | </ | ||
+ | |||
+ | <WRAP center round important 60%> | ||
+ | |||
+ | You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD3029LZ platform. | ||
+ | |||
+ | </ | ||
+ | |||
+ | ===== Downloading the ADuCM302x Software Pack ===== | ||
+ | |||
+ | The software pack can be installed directly by the tool chain' | ||
+ | - Downloaded via the tool chain' | ||
+ | * It is **recommended** to download the ADuCM302x software pack through from the tool chain' | ||
+ | - Downloaded to local directory | ||
+ | * However if you do decide to download the ADuCM302x software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to " | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | |||
+ | [[http:// | ||
+ | |||
+ | </ | ||
+ | |||
+ | // End of Document // | ||
+ | |||
+ | **[[resources: |