EVAL-CN0363-PMDZ Hardware Setup
The CN0363 HDL reference design and software are designed to operate with the following hardware and FPGA development system:
The equipment should be connected as shown below, make sure that all power is off before starting to make the connections.
PMOD JA connector of the ZED board connected to the PMOD connector on the EVAL-CN0363-PMDZ
USB mouse and keyboard connected to the ZED board (J13)
12
V power supply connected to the ZED board (J20)
Ethernet cable with internet connection connected to the ZED board (only required for software updates)
HDMI monitor connected to the ZED board (J9)
SD card inserted into the ZED board (J12)
6V to 12V power supply connected to the EVAL-CN0363-PMDZ