Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:eval-cn0363-pmdz:hardware [24 May 2018 01:44] Jesse Daniel Santosresources:eval:user-guides:eval-cn0363-pmdz:hardware [24 May 2018 02:25] (current) Jesse Daniel Santos
Line 7: Line 7:
 Interfaced with EVAL-CN0363-PMDZ is an FPGA development board ([[http://zedboard.org/product/zedboard|ZED Board]] rev C or later). Zedboard requires a separate 12V DC power supply connected to its DC power jack. Interfaced with EVAL-CN0363-PMDZ is an FPGA development board ([[http://zedboard.org/product/zedboard|ZED Board]] rev C or later). Zedboard requires a separate 12V DC power supply connected to its DC power jack.
  
-{{:resources:eval:user-guides:eval-cn0363-pmdz:zed_brd_pwr.jpg?300|}}+{{:resources:eval:user-guides:eval-cn0363-pmdz:zed_brd_pwr.jpg?400|}}\\ 
 + 
 +======IOVDD Provisions====== 
 +EVAL-CN0363-PMDZ provides two options of IOVDD using header <fc #ff0000>JP1</fc>. If pin 1 and pin 2 is shorted, IOVDD comes from the regulated supply of the board. If pin 2 and pin 3 is shorted, IOVDD comes from the PMOD interface.\\ 
 + 
 +{{:resources:eval:user-guides:eval-cn0363-pmdz:cn0363_iovdd_1.jpg?400|}}\\
  
 =====Input Interface===== =====Input Interface=====
resources/eval/user-guides/eval-cn0363-pmdz/hardware.txt · Last modified: 24 May 2018 02:25 by Jesse Daniel Santos