This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adxl355-pmdz:no-os-setup [27 Sep 2022 17:20] – fix backlink, moved no-os:overview to no-os Darius B | resources:eval:user-guides:eval-adxl355-pmdz:no-os-setup [14 Feb 2023 09:55] (current) – [Aducm3029 Platform] Ramona Bolboaca | ||
---|---|---|---|
Line 89: | Line 89: | ||
| Pin 6 | POWER 3.3V | Digital Power | VDD | | | Pin 6 | POWER 3.3V | Digital Power | VDD | | ||
| Pin 10 | P1_9 | Data Ready | DRDY | | | Pin 10 | P1_9 | Data Ready | DRDY | | ||
+ | |||
+ | |||
+ | ==== Aducm3029 Platform ==== | ||
+ | === Hardware Setup === | ||
+ | == Required Hardware == | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | == Required Connections == | ||
+ | The [[ADI> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Pico Platform ==== | ||
+ | === Hardware Setup === | ||
+ | == Required Hardware == | ||
+ | * [[ADI> | ||
+ | * [[https:// | ||
+ | == Required Connections == | ||
+ | The [[https:// | ||
+ | The following table shows how the connection between [[ADI> | ||
+ | |||
+ | ^ P1 EVAL-ADXL355-PMDZ Pin Number ^ RPI Pico Pin Number ^ Function ^ Mnemonic ^ | ||
+ | | Pin 1 | GP17 | Chip Select | ||
+ | | Pin 2 | GP19 | Master Out Slave In | MOSI | | ||
+ | | Pin 3 | GP16 | Master In Slave Out | MISO | | ||
+ | | Pin 4 | GP18 | Serial Clock | SCLK | | ||
+ | | Pin 5 | GND | Digital Ground | ||
+ | | Pin 6 | 3.3V | Digital Power | VDD | | ||
+ | | Pin 10 | GP20 | Data Ready | DRDY | | ||
+ | |||
+ | |||
===== No-OS Build Setup ===== | ===== No-OS Build Setup ===== |