This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:eval-adxl313z:no-os-setup [03 Jun 2022 13:14] George Mois [IIO Project] |
resources:eval:user-guides:eval-adxl313z:no-os-setup [27 Sep 2022 17:20] Darius B fix backlink, moved no-os:overview to no-os |
||
---|---|---|---|
Line 32: | Line 32: | ||
The goal of ADI Microcontroller No-OS is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. ADI No-OS offers **generic drivers** which can be used as a base for any microcontroller platform and also **example projects** which are using these drivers on various microcontroller platforms. | The goal of ADI Microcontroller No-OS is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. ADI No-OS offers **generic drivers** which can be used as a base for any microcontroller platform and also **example projects** which are using these drivers on various microcontroller platforms. | ||
- | For more information about ADI No-OS and supported microcontroller platforms see: [[:resources:no-os:overview | ADI No-OS]]. | + | For more information about ADI No-OS and supported microcontroller platforms see: [[:resources:no-os | no-OS]]. |
===== ADXL313 Driver ===== | ===== ADXL313 Driver ===== |