This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adtf3175d-nxz:system_update [07 Feb 2023 20:01] – [Firmware Update] Andre Straker-Payne | resources:eval:user-guides:eval-adtf3175d-nxz:system_update [25 Apr 2023 18:42] – Update to version information. Andre Straker-Payne | ||
---|---|---|---|
Line 9: | Line 9: | ||
In general the data_collect executable is used to update the firmware. This can be done from the host or on the device. | In general the data_collect executable is used to update the firmware. This can be done from the host or on the device. | ||
- | The firmware binary file for the latest version is available on the respective flash image. The binary file can be also obtained from the ADSD3500 installer. From the installer package, under the directory ADSD3500_Release_Firmware, | + | The firmware binary file for the latest version is available on the respective flash image. The binary file can be also obtained from the ADSD3500 installer. From the installer package, under the directory ADSD3500_Release_Firmware, |
- | * Fw_Update_4.1.0.bin | + | * Fw_Update_4.1.5.bin |
On the device: | On the device: | ||
< | < | ||
cd ~/Eval/bin | cd ~/Eval/bin | ||
- | ./ | + | ./ |
</ | </ | ||
From the host: | From the host: | ||
< | < | ||
- | cd " | + | cd " |
- | data_collect --fw Fw_Update_4.1.0.bin --ip 10.42.0.1 tof-viewer_config.json | + | data_collect --fw Fw_Update_4.1.5.bin --ip 10.42.0.1 tof-viewer_config.json |
</ | </ | ||
+ | |||
+ | In either case wait for 60s before restarting the system. | ||
===== Full Flash/NVM Update ===== | ===== Full Flash/NVM Update ===== | ||
Line 28: | Line 30: | ||
Updating the full flash should only be done if absolutely needed. | Updating the full flash should only be done if absolutely needed. | ||
- | |||
- | ==== Generating the Flash Image ==== | ||
- | |||
- | |||
- | |||
- | ==== Programming the Flash ==== | ||
<note important> | <note important> |