Wiki

This version is outdated by a newer approved version.DiffThis version (16 Aug 2021 14:44) was approved by Harshvardhan Bhatia.The Previously approved version (01 Aug 2021 19:50) is available.Diff

This is an old revision of the document!


EVAL-ADSD3100-NXZ Startup Guide

Kit Contents

  • ADSD3100-NXZ Evaluation Module
    • ADSD3100 Imager Module
    • i.MX8 M Plus SOM (SolidRun)
    • Camera Interface Board
  • 16GB flashed microSD card (Inserted in module sd card slot)
  • Anker USB Hub
  • USB-C to USB-C cable. Supports PD 2.0, and USB 3.1

Software Download

  • GUI Install Guide: link

Startup

  • Connect USB-C cable to module

  • Connect USB-C to laptop
  • Wait for green light under the USB-C connector on the module light up
  • Run GUI
If mp_pcm mode does not work (ie. GUI is stuck/crashes), disconnect USB-C Cable from laptop. Connect module to USB-C hub 5Gbps port (highlighted by white box), and connect hub to pc. Restart the GUI and try again.

Troubleshooting

  • GUI Crash
    • Ensure that that mode switching is done after module is stopped
    • If the GUI is always crashing, particularly for mp_pcm, the module is likely not getting enough power. If adding the hub did not fix the issue, it is likely that the host port does not support the power requirements.
  • Green light under USB-C Connector not turning on
    • SD-Card could be corrupted. 'Firmware Flashing Link'
resources/eval/user-guides/eval-adsd3100-nxz-startup.1629117857.txt.gz · Last modified: 16 Aug 2021 14:44 by Harshvardhan Bhatia