This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adsd3100-nxz-software-installation [31 Oct 2022 21:44] – [Download Installer] Harshvardhan Bhatia | resources:eval:user-guides:eval-adsd3100-nxz-software-installation [09 Nov 2022 17:58] – [Image Folder Contents] Harshvardhan Bhatia | ||
---|---|---|---|
Line 48: | Line 48: | ||
==== Image Folder Contents ==== | ==== Image Folder Contents ==== | ||
{{ : | {{ : | ||
+ | |||
+ | * microsd-xxxxxxxx : NXP SOM sd card image | ||
+ | * Flashing instructions : [[: | ||
+ | |||
+ | * fwUpdate_X.X.X : This is the ADSD3500 firmware | ||
+ | * Update instructions here : [[: | ||
+ | | ||
* depth_compute : Contains depth compute binaries | * depth_compute : Contains depth compute binaries | ||
* More information : [[: | * More information : [[: | ||
- | * fwUpdate_X.X.X : This is the ADSD3500 firmware | ||
- | * Update instructions here : [[: | ||
- | * microsd-xxxxxxxx : NXP SOM sd card image | ||
- | * Flashing instructions : [[: | ||
+ | Correct update procedure: | ||
+ | * Update NXP SOM sd-card image | ||
+ | * Run fw update to update ADSD3500 firmware | ||
==== Done ==== | ==== Done ==== |