This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision Last revision Both sides next revision | ||
resources:eval:user-guides:eval-adsd3100-nxz-gui [07 Jul 2022 20:36] Harshvardhan Bhatia [Run Camera] |
resources:eval:user-guides:eval-adsd3100-nxz-gui [07 Dec 2022 17:04] Harshvardhan Bhatia |
||
---|---|---|---|
Line 6: | Line 6: | ||
==== Start ==== | ==== Start ==== | ||
+ | |||
+ | |||
* Find the ADIToFGUI.exe in the 'viewer' or 'bin' folder located at the install location | * Find the ADIToFGUI.exe in the 'viewer' or 'bin' folder located at the install location | ||
* v2.x.x | * v2.x.x | ||
Line 11: | Line 13: | ||
* v3.x.x | * v3.x.x | ||
* Default location : C:\Analog Devices\TOF_Evaluation_BM-RelX.X.X\bin\ | * Default location : C:\Analog Devices\TOF_Evaluation_BM-RelX.X.X\bin\ | ||
+ | * If you are evaluating the **EVAL-ADTF3175D-NXZ**: | ||
+ | * Confirm that an unidentified local network has been discovered by the pc - IP address = 10.42.0.1 | ||
+ | * Run TOF_Evaluation_BM-Rel3.x.x | ||
+ | * Hit refresh until a Device is found | ||
+ | * Select **tof-viewer_config.json** config file in the drop down menu, and hit 'Open Device' | ||
* If you are evaluating the following modules : **EVAL-ADTF3175-NXZ** or **EVAL-ADSD3100-NXZ** | * If you are evaluating the following modules : **EVAL-ADTF3175-NXZ** or **EVAL-ADSD3100-NXZ** | ||
- | * Run TOF_Evaluation_BM-Rel2.x.x, you should see the window below | ||
* Start the viewer to get to the window below | * Start the viewer to get to the window below | ||
- | * If a camera is connected it should show up in the 'Device' drop down menu | + | * If a camera is connected it should show up in the 'Device' drop down menu |
- | * Select your device | + | * Select your device |
- | * Select correct config file (depends on which module you are using) | + | * Select correct config file (depends on which module you are using) |
- | * [[:resources:eval:user-guides:eval-adtf3175-nxz| EVAL-ADTF3175-NXZ]] : tof-viewer-config-adtf3175 | + | * [[:resources:eval:user-guides:eval-adtf3175-nxz| EVAL-ADTF3175-NXZ]] : **tof-viewer-config-adtf3175.json** |
- | * [[:resources:eval:user-guides:eval-adsd3100-nxz| EVAL-ADSD3100-NXZ]] : tof-viewer-config-adsd3100 | + | * [[:resources:eval:user-guides:eval-adsd3100-nxz| EVAL-ADSD3100-NXZ]] : **tof-viewer-config-adsd3100.json** |
- | * Click 'Open Device' | + | * Click 'Open Device' |
- | * If you are evaluating the **EVAL-ADTF3175D-NXZ** | + | |
- | * Confirm that an unidentified local network has been discovered by the pc - IP address = 10.42.0.1 | + | |
- | * Run TOF_Evaluation_BM-Rel3.x.x, the GUI should stay on. | + | |
- | * If the GUI automatically turns off, or takes too long to start, it is likely that the camera server is not detected, please visit the troubleshooting guide | + | |
- | * Select tof-viewer_config config file in the drop down menu, and hit 'Open Device' | + | |
{{ :resources:eval:user-guides:selecting_config.png?nolink |}} | {{ :resources:eval:user-guides:selecting_config.png?nolink |}} |