resources:eval:user-guides:eval-adsd3100-nxz-gui [01 Aug 2021 11:46]
Harshvardhan Bhatia Initial Info
resources:eval:user-guides:eval-adsd3100-nxz-gui [01 Aug 2021 14:01]
Harshvardhan Bhatia [ADSD3100 GUI/Viewer Guide]
Line 1: Line 1:
-====== ​ADSD3100 GUI/Viewer Guide ====== +====== ​ADIToFGUI ​====== 
-This is a guide for the ToF viewer. ​+This is a guide for the ToF module ​viewer. ​
  
  
Line 21: Line 21:
   * If this option is selected, the first window will show active brightness/​intensity,​ while the second window will show depth   * If this option is selected, the first window will show active brightness/​intensity,​ while the second window will show depth
   * Depth is shown in mm, the user can hover over the image to see real-time depth data   * Depth is shown in mm, the user can hover over the image to see real-time depth data
 +{{ :​resources:​eval:​user-guides:​ab_and_depth.png?​nolink |}}
  
 +==== Mode Switching ====
 +  * If the user wants to switch modes while the camera is running frames:
 +    * Click '​Stop'​
 +    * Select mode in drop down menu
 +    * Click '​Play'​
  
 ==== Point Cloud and Depth ==== ==== Point Cloud and Depth ====
Line 29: Line 35:
     * Click '​Play'​     * Click '​Play'​
   * If this option is selected, the first window will show a point-cloud generated from the depth on the second window.   * If this option is selected, the first window will show a point-cloud generated from the depth on the second window.
-  * The user can orient ​the point cloud by dragging ​the mouse while holding ​the right mouse button +  * Point Cloud Controls: 
-  Click 'Reset View' in the point cloud window to reset the orientation+    * Zoom In/Out 
 +      * Use the mouse wheel and scroll forward to zoom in, scroll backwards to zoom out. 
 +    * Grab image and move it in all directions 
 +      * Hover over the Point Cloud Image and and drag the mouse while the right mouse button ​is pressed. Move slowly 
 +    Rotate image 
 +      * Drage the mouse while pressing the left mouse button 
 +    * Increase / Decrease Point Cloud point size  
 +      * Grab the slider at the bottom of the Point Cloud window ​and move it left or right to decrease or increase ​the point size 
 +    * Reset View 
 +      * Press the “Reset View” button to restore to default image size and position
  
 {{ :​resources:​eval:​user-guides:​adsd3100_viewer_pc_and_depth.png?​nolink |}} {{ :​resources:​eval:​user-guides:​adsd3100_viewer_pc_and_depth.png?​nolink |}}
 +
 +==== Recording ====
 +  * Recording option allows users to save AB, Depth, and PointCloud, and raw frames while viewing the scene
 +  * Select the number of frames to record and click 'Start Recording'​
 +  * In the pop-up window select save location and file format:
 +    * .raw - 
 +    * .fsf -
 +
 +==== Playback ====
 +  * The '​Playback Options'​ menu allows the user to play recorded data
 +  * Click 'Open Recording'​ and select either a '​.raw'​ file or an '​_XYZ.fsf'​ file
 +
 +
 +===== Troubleshooting =====
 +  * Camera not showing up on drop down menu
 +    * Click '​Refresh Devices'​ to get updated list
 +    * Disconnect the camera and quit GUI
 +    * Connect the camera and ensure it shows up on Device Manager
 +    * Start GUI
 +  * GUI stuck
 +    * Typically occurs when mode switching fails. Restart GUI and power cycle camera
 +    * Ensure that camera playback is stopped before switching modes
  
resources/eval/user-guides/eval-adsd3100-nxz-gui.txt · Last modified: 01 Aug 2021 14:01 by Harshvardhan Bhatia