This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adsd3100-nxz-gui [01 Aug 2021 11:46] – Initial Info Harshvardhan Bhatia | resources:eval:user-guides:eval-adsd3100-nxz-gui [01 Aug 2021 12:22] – Updated mode switching and troubleshooting Harshvardhan Bhatia | ||
---|---|---|---|
Line 21: | Line 21: | ||
* If this option is selected, the first window will show active brightness/ | * If this option is selected, the first window will show active brightness/ | ||
* Depth is shown in mm, the user can hover over the image to see real-time depth data | * Depth is shown in mm, the user can hover over the image to see real-time depth data | ||
+ | {{ : | ||
+ | ==== Mode Switching ==== | ||
+ | * If the user wants to switch modes while the camera is running frames: | ||
+ | * Click ' | ||
+ | * Select mode in drop down menu | ||
+ | * Click ' | ||
==== Point Cloud and Depth ==== | ==== Point Cloud and Depth ==== | ||
Line 29: | Line 35: | ||
* Click ' | * Click ' | ||
* If this option is selected, the first window will show a point-cloud generated from the depth on the second window. | * If this option is selected, the first window will show a point-cloud generated from the depth on the second window. | ||
- | * The user can orient | + | * Point Cloud Controls: |
- | * Click 'Reset View' in the point cloud window to reset the orientation. | + | * Zoom In/Out |
+ | * Use the mouse wheel and scroll forward to zoom in, scroll backwards to zoom out. | ||
+ | * Grab image and move it in all directions | ||
+ | * Hover over the Point Cloud Image and and drag the mouse while the right mouse button | ||
+ | * Rotate image | ||
+ | * Drage the mouse while pressing the left mouse button | ||
+ | * Increase / Decrease Point Cloud point size | ||
+ | * Grab the slider at the bottom of the Point Cloud window | ||
+ | * Reset View | ||
+ | * Press the “Reset View” button to restore to default image size and position | ||
{{ : | {{ : | ||
+ | |||
+ | ==== Recording ==== | ||
+ | * Recording option allows users to save AB, Depth, and PointCloud, and raw frames while viewing the scene | ||
+ | * Select the number of frames to record and click 'Start Recording' | ||
+ | * In the pop-up window select save location and file format: | ||
+ | * .raw - | ||
+ | * .fsf - | ||
+ | |||
+ | ==== Playback ==== | ||
+ | * The ' | ||
+ | * Click 'Open Recording' | ||
+ | |||
+ | |||
+ | ===== Troubleshooting ===== | ||
+ | * Camera not showing up on drop down menu | ||
+ | * Click ' | ||
+ | * Disconnect the camera and quit GUI | ||
+ | * Connect the camera and ensure it shows up on Device Manager | ||
+ | * Start GUI | ||
+ | * GUI stuck | ||
+ | * Typically occurs when mode switching fails. Restart GUI and power cycle camera | ||
+ | * Ensure that camera playback is stopped before switching modes | ||