This is an old revision of the document!
Data Collect Command Line Interface (CLI)
Description
The Data Collect CLI can collect raw data from the depth module in .bin format. This be run through the Depth Compute CLI to convert to Depth, IR/AB(Active brightness), and XYZ frames
Flag descriptions:
--f : output data folder
--n : number of frames captured
--
m : mode (7 - qmp, 10 - mp)
--wt : warmup time (seconds)
--ccb : stores ccb (Calibration parameters) file stored on NVM of imager module. Required for Depth Compute
--h : Call help string for all options
More information can be found in readme
EVAL-ADSD3100-NXZ and EVAL-ADTF3175-NXZ Example
Capture 1 mp frame
Open Command Prompt from start menu and move to data_collect folder in
GUI install location.
Run data_collect executable : data_collect.exe --f “../data_output” --
m 10 --n 4 --ccb ../crXXX.ccb tof-viewer-config-adtf3175.json
The .json file selected must correspond to your module:
EVAL-ADTF3175D-NXZ Example
Since the ADTF3175D eval kit works via ethernet over usb, the useer must specify the static ip of the camera module
Mode 10, 1 frame capture, get ccb
data_collect.exe --f “data_output” --
m 10 --n 1 --ccb ../crXXX.ccb --ip 10.42.0.1 tof-viewer_config.json
The get ccb flag is only required for the first capture. Once the ccb of your module is stored, it can be reused while running tofi_depth_compute.exe