This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adsd3100-nxz-gui:datacollect_cli [07 Jul 2022 20:45] – Harshvardhan Bhatia | resources:eval:user-guides:eval-adsd3100-nxz-gui:datacollect_cli [07 Jul 2022 20:46] – [EVAL-ADTF3175D-NXZ Example] Harshvardhan Bhatia | ||
---|---|---|---|
Line 16: | Line 16: | ||
====EVAL-ADSD3100-NXZ and EVAL-ADTF3175-NXZ Example==== | ====EVAL-ADSD3100-NXZ and EVAL-ADTF3175-NXZ Example==== | ||
Capture 1 mp frame | Capture 1 mp frame | ||
- | * Open Command Prompt from start menu and move to data_collect | + | * Open Command Prompt from start menu and move to bin folder in GUI install location. |
* Run the following command : (Mode 10 - MP, 1 frame capture, get ccb) | * Run the following command : (Mode 10 - MP, 1 frame capture, get ccb) | ||
* data_collect.exe --f " | * data_collect.exe --f " | ||
Line 31: | Line 31: | ||
Since the ADTF3175D eval kit works via ethernet over usb, the user must specify the static ip of the camera module | Since the ADTF3175D eval kit works via ethernet over usb, the user must specify the static ip of the camera module | ||
- | * Open Command Prompt from start menu and move to data_collect | + | * Open Command Prompt from start menu and move to bin folder in GUI install location. |
* Run the following command (Mode 10, 1 frame capture, get ccb): | * Run the following command (Mode 10, 1 frame capture, get ccb): | ||
* data_collect.exe --f " | * data_collect.exe --f " |