This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adsd3100-nxz-gui:datacollect_cli [07 Jul 2022 20:46] – [EVAL-ADSD3100-NXZ and EVAL-ADTF3175-NXZ Example] Harshvardhan Bhatia | resources:eval:user-guides:eval-adsd3100-nxz-gui:datacollect_cli [07 Jul 2022 20:46] – [EVAL-ADTF3175D-NXZ Example] Harshvardhan Bhatia | ||
---|---|---|---|
Line 31: | Line 31: | ||
Since the ADTF3175D eval kit works via ethernet over usb, the user must specify the static ip of the camera module | Since the ADTF3175D eval kit works via ethernet over usb, the user must specify the static ip of the camera module | ||
- | * Open Command Prompt from start menu and move to data_collect | + | * Open Command Prompt from start menu and move to bin folder in GUI install location. |
* Run the following command (Mode 10, 1 frame capture, get ccb): | * Run the following command (Mode 10, 1 frame capture, get ccb): | ||
* data_collect.exe --f " | * data_collect.exe --f " |