The connections between the Servo Motor and the ADPAQ module are made as shown below.
Servo motor Pins
GPIO port used
ADPAQ Header Pins
A
5V
P2-1
B
P0_1
P2-5
C
GND
P2-10
Build and run the project
The tile has a “Freq” button and an input value option. We can set the frequency of the servo any value between 0-100 and the servo motor rotates accordingly.image
resources/eval/user-guides/eval-adpaq3029/resources/app_servo.txt · Last modified: 06 Nov 2018 05:37 by Sundar Palani