Please see the resource section to download source code.
File
→ Import..
or click Import an existing CCES project
from homepage as shown below. General
→ Existing Projects into Workspace
.
The module application runs on the bootloader and the MDK provides APIs required for communication with the gateway. The bootloader and the MDK projects have to be added to the workspace. They can be downloaded from the resource page along with application source code. To add them to the workspace, follow the procedure described as above.
Properties
.C/C++ Build
→ Settings
→ Cross Core GCC ARM Embedded C Linker
→ Libraries
.add
(at the top right section inside settings tab) and then File system
. Then search for the required files from the workspace and add them. imageC:\Users\psirivan\Desktop
is the path to the workspace, 6Feb6
is the name of the workspace.nosys.specs
, as shown in the figure below.