This page provides all the necessary steps to get CrossCore Embedded Studio (CCES) software environment up and running on Windows or Linux.
The CCES software development environment for EVAL-ADICUP360 is based on open source tools, and is maintained by Analog Devices. CCES includes support for DSP (digital signal processing) and ARM Cortex M- and A- devices, and includes the following features and many more:
-
GNU ARM Embedded Toolchain for Cortex-
M core based parts (6-2017-q2-update release)
OpenOCD with support for Cortex-
M microcontroller (open source SWD)
CMSIS Pack files
Mbed CMSIS-DAP
J-Link Lite
CrossCore Embedded Studio is based on
Eclipse, but because the MBED platform provides a CMSIS-DAP interface to connect to the board, the EVAL-ADICUP360 can be used without problems with
IAR Embedded Workbench IDE or
Keil µVision IDE as well.
Pre-Requisites and Requirements List
There are a few things that you will need for the tools and software to work properly.
PC or laptop computer
EVAL-ADICUP360 hardware
-
USB cable needs to have ALL data lines connected, can't use a charging only micro
USB cable.
CrossCore Embedded Studio Download Packages
The following features are available and supported
The following features are only supported via the Windows version
CrossCore Embedded Studio Installer Instructions
It is best that you save all the files/folders to the default directories recommended by the CrossCore Embedded Studios installer. This way all the instructions and support provided will be easier.
Installing CrossCore Embedded Studio on Windows
The executable installs all necessary components to the Analog Devices local directory structure which can be found below.
CrossCore Embedded Studio installs to C:\Analog Devices\CrossCore Embedded Studio 2.8.0
Eclipse
IDE installs to
C:\Analog Devices\CrossCore Embedded Studio 2.8.0\Eclipse
GNU ARM Embedded Toolchain for Cortex-
M installs to
C:\Analog Devices\CrossCore Embedded Studio 2.8.0\ARM\gcc-arm-embedded
OpenOCD installs to C:\Analog Devices\CrossCore Embedded Studio 2.8.0\ARM\openocd\bin
CMSIS Pack files are installed to C:\Analog Devices\CrossCore Embedded Studio 2.8.0\ARM\packs
Installing CrossCore Embedded Studio on Linux
CrossCore Embedded Studio can be installed and used on Ubuntu 14.04+ 32-bit and 64-bit.
The Ubuntu Linux Installer(Debian) installs all necessary components to the Analog Devices local directory structure which can be found below.
CrossCore Embedded Studio installs to /opt/analog/cces/2.8.0
Eclipse
IDE installs to
/opt/analog/cces/2.8.0/Eclipse
GNU ARM Embedded Toolchain for Cortex-
M installs to
/opt/analog/cces/2.8.0/ARM/gcc-arm-embedded
OpenOCD installs to /opt/analog/cces/2.8.0/ARM/openocd/bin
CMSIS Pack files are installed to /opt/analog/cces/2.8.0/ARM/packs
Activating CrossCore Embedded Studio
The first time you launch CrossCore Embedded Studio, you will be prompted to input a serial number, name, and email address. The serial number for ALL EVAL-ADICUP360 boards is:
EVAL-ADICUP360 CrossCore Serial Number
EZK-CCES-5JNP-FQH2-IAZZ-IJY4-E4HG-YIY6-JE01
The New License Wizard will guide you through the process.
Select Yes to install a license at this time.
Choose “I have a serial number that I would like to activate” and click Next.
Enter the serial number above ( EZK-CCES-5JNP-FQH2-IAZZ-IJY4-E4HG-YIY6-JE01 ) and click Next.
Choose “Install and activate a license on-line all in one step” and click Next.
Complete your name and address and click Finish.
On success, you will be prompted with a dialog that tells you that “Your license has been successfully activated”. Click OK.
Once the serial number has been activated, the CrossCore development tools will allow you full and unlimited access to all the features of the tool when using the Analog Devices family of ARM Cortex Processor.
CrossCore Embedded Studio Support
For more details on CrossCore Embedded Studio, updated versions of the tools, release notes, tools documentation, or other support. Please visit the CrossCore webpage, or email the CrossCore support team at processor.tools.support@analog.com
End of Document