Wiki

This version is outdated by a newer approved version.DiffThis version (14 Jan 2021 05:32) was approved by Robin Getz.The Previously approved version (03 Jan 2021 21:46) is available.Diff

This is an old revision of the document!


Total Dissolved Solids Measurements Demo

The ADuCM360_demo_cn0411 is a Total Dissolved Solids (TDS) measurements demo project, for the EVAL-ADICUP360 base board with additional EVAL-CN0411-ARDZ shield, created using the GNU ARM Eclipse Plug-ins in Eclipse environment.

General Description/Overview

The ADuCM360_demo_cn0411 project uses the EVAL-CN0411-ARDZ shield which is a single supply, low power, high precision complete solution for Total Dissolved Solids measurements, including temperature compensation. The circuit is optimized for conductivity measurements used to determine the TDS values, using conductivity cells with BNC plug.

The circuit is divided into three independent measurement front ends: TDS, conductivity and temperature. After signal conditioning, the three channels share an AD7124-8, 24-bit sigma-delta (Σ-Δ) ADC. The AD7124-8, is a low power, low noise, completely integrated analog front end for high precision measurement applications.

For temperature compensation can be used an RTD PT100 sensor, 2-wire. The ADuCM360_demo_cn0411 application processes ADC outputs for all 5 channels (RTD, Vpeak+ and Vpeak-, VDAC, VR20S, VR200S), calculates conductivity and TDS values using as input RTD temperature value and the peak-to-peak voltage. Those data are sent to serial interface, using UART communication (115200 baud rate and 8-bits data length). The 24-bits ADC data are received using SPI interface of the EVAL-ADICUP360 board.


The temperature value is calculated based on the RTD resistance:

                                                               
       Rrtd = (CODE* Rref) / (2^24 -1)                         Rref - Reference resistor (4.02kΩ)        
                                                               CODE - ADC output
                                                               


1. RTD resistance > 100Ω


2. RTD resistance ≤ 100Ω


In order to compute the total dissolved solids parameter a premeasurement procedure is run in the first place that aims to select the proper gain resistance for the measurement.

The multiplexer is set to the highest gain resistance (20MΩ) and the DAC output to a value set by the user (initially set to 400mV). Then, the positive and negative input voltage are captured via ADC channel 1 and 2. If the following formula is met:

                                                Vp = positive input voltage
       Vp + Vn > 0.3 * 2 * Vexc                 Vn = negative input voltage
                                                Vexc = DAC output voltage

The excitation voltage used for computing tds is set to:

                                                                       
       Vexc = 0.4 * Vexc / (Vp + Vn)      
                                                                      

Otherwise, the gain resistor is dropped by 1 decade and the premeasurement process is repeated.

After the process is finished, the peak-to-peak voltage is measured again an the peak-to-peak current is computed:

                                                  Ipp = peak-to-peak current              
       Ipp = (2 * Vexc - (Vp + Vn)) / Rgain       Vexc = excitation voltage computed in the premeasurement procedure
                                                  Vp = positive input voltage
                                                  Vn = negative input voltage
                                                  Rgain = gain resistor set via multiplexer    
                                                                  

Based on the peak-to-peak current the electrical conductance is computed, also removing the offset resistance (optional) that is obtained via the software command “refres” found in the list of available commands :

                                                  
       g = Ipp / ((Vp + Vn) - (Ipp * Roff))       Roff = offset resistance    
                                                  g = electrical conductance
       

The electrical conductivity is computed using the conductance and the cell constant which can be set accordingly for low conductivities, normal conductivities and high conductivities via software commands. A temperature compensation is also performed taking into account the temperature measured via RTD resistance.

                                                          s = electrical conductivity
       s = k * g                                          s_cal = temperature compensated electrical conductivity
                                                          temp_coeff = solution temperature coefficient 
       s_cal = s / (1 + temp_coeff * (temp - t_cal))      temp = measured temperature
                                                          t_cal = reference temperature (25°C)
                                                  

The calculation of total dissolved solids is the product between the temperature compensated conductivity and the tds factor corresponding to the solution that is used.

       tds = k_e * s_cal                                  k_e = tds factor
                                                          tds = total dissolved solids
       

Demo Requirements

The following is a list of items needed in order to replicate this demo.

  • Hardware
    • EVAL-ADICUP360
    • EVAL-CN0411-ARDZ
    • Conductivity cell with BNC Connector
    • PT100/PT1000 RTD probe
    • Mirco USB to USB cable
    • PC or Laptop with a USB port
  • Software
    • ADuCM360_demo_CN0411 software
    • CrossCore Embedded Studio (2.7.0 or higher)
    • ADuCM36x DFP (1.0.2 or higher)
    • CMSIS ARM Pack (4.3.0 or higher)
    • Serial Terminal Program
      • Such as Putty or Tera Term

Setting up the Hardware

  1. To program the base board, set the jumpers/switches as shown in the next figure. The important jumpers/switches are highlighted in red.
  1. Connect the EVAL-CN0411-ARDZ Shield to the Arduino connectors P2, P5, P6, P7, P8 of the EVAL-ADICUP360 board.
  2. Connect the conductivity cell to the J1 connector of the EVAL-CN0411-ARDZ.
  3. Connect the RTD sensor to the P3 connector of the EVAL-CN0411-ARDZ.
  4. Connect PIN1 and PIN2 on P5 connector and PIN1 and PIN2 on P6 connector to read data from the conductivity cell.
  5. Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14)

Obtaining the Source Code

We recommend not opening the project directly, but rather import it into CrossCore Embedded Studios and make a local copy in your workspace.

The source code and include files of the ADuCM360_demo_cn0411 can be found here:


CrossCore Embedded Studio Application Source Code:

AduCM360_demo_cn0411 at Github

For more information on importing, debugging, or other tools related questions, please see the tools user guide.

Configuring the Software Parameters

  • DAC default output value - DAC_OUT_DEFAULT_VAL - set default output voltage for the DAC. (CN0411.h).
   #define DAC_OUT_DEFAULT_VAL     0.4
  • KCl solution TDS factor - TDS_KCL - set the TDS factor for the KCl solution. (CN0411.h).
   #define  TDS_KCL                0.5
  • NaCl solution TDS factor - TDS_NACL - set the TDS factor for the NaCL solution. (CN0411.h).
   #define  TDS_NACL               0.47
  • KCl solution temperature coefficient - TEMP_COEFF_KCL - set the temperature coefficient for the KCl solution. (CN0411.h).
   #define  TEMP_COEFF_KCL         1.88
  • NaCl solution temperature coefficient - TEMP_COEFF_NACL - set the temperature coefficient for the NaCl solution. (CN0411.h).
   #define  TEMP_COEFF_NACL        2.14

Outputting Data

Serial Terminal Output

  1. In order to view the data, you must flash the program to the EVAL-ADICUP360.
  2. Once complete you will need to switch the USB cable from the DEBUG USB (P14) to the USER USB (P13).
  3. Then follow the UART settings below with the serial terminal program.


Following is the UART configuration.

  Select COM Port
  Baud rate: 115200
  Data: 8 bit
  Parity: none
  Stop: 1 bit
  Flow Control: none


  • The user must press the <ENTER> key to start the program.
  • To get to the command menu the user must type <help> into the serial program.
  • Semihosting must be enabled to see data at the console window.

Available commands

Command Description
help Display available commands
syscal Perform ADC system zero-scale calibration. Before calibration, short terminals 5 & 6 in jumper P5.
refres Perform Referencing to a Precision Resistance. Before referencing, short terminals 3 & 4 in jumper P5.
convmod(sing/cont) set single/continuous conversion mode for ADC.
autoset Autoset Gain Resistance.
setdac<val> Set DAC value (Volts).
gainres <val> Set Gain Resistor value (Ω). <val> = 20/200/2K/20K/200K/2M/20M
rtdval <val> Set RTD value (Ω). <val> = values 100, 1000
pwmfreq <val> Set PWM frequency value (Hz), <val> = values 94, 2400
cellconst (low/normal/high/<val>) Set cell constant for conductivity types.
solution (kcl/nacl/<val_tmp_coeff,val_tds_factor>) Set parameters for specific solution.
temp Display temperature value.
vinput (pos/neg) Display Positive/Negative input voltage.
readdac Read DAC value (Volts).
rdr20s Read Voltage on R20S (Volts).
rdr200s Read Voltage on R200S (Volts).
readdac Read DAC value (Volts).
readdac Read DAC value (Volts).
rdres Read Input Resistance (Volts).
cond Display conductivity value.
tds Display TDS value.

How to use the Tools

The official tool we promote for use with the EVAL-ADICUP360 is CrossCore Embedded Studio. For more information on downloading the tools and a quick start guide on how to use the tool basics, please check out the Tools Overview page.

Importing

For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to import existing projects into your workspace section.

Debugging

For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to configure the debug session section.

Project Structure

The ADuCM360_demo_cn0411 is a C++ project that uses ADuCM36x C/C++ Project structure.

This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripherals; port configuration for ADC, SPI read/write; for configuring and reading from AD7124, UART via P0.6/P0.7; UART read/write functions; for calibration and displaying the results.

In the src and include folders you will find the source and header files related to CN0411 software application. The Communication.c files contain SPI and UART specific data, meanwhile the CN0411.c files contain the calculation part, the AD7124.c files contain ADC channels handling. The default parameters are set at the run time, after initialization in the terminal window will appear information messages about the initial setup.

The RTE folder contains device and system related files:

  • Device Folder – contains low levels drivers for ADuCM360 microcontroller.(try not to edit these files)
  • system.rteconfig - Allows the user to select the peripherial components they need, along with the startup and ARM cmsis files needed for the project.



End of Document

resources/eval/user-guides/eval-adicup360/reference_designs/demo_cn0411.1610598244.txt.gz · Last modified: 14 Jan 2021 05:24 by Robin Getz