Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0411 [14 Jan 2021 05:24] – use / interwiki links Robin Getzresources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0411 [14 Mar 2021 10:12] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo
Line 130: Line 130:
   - Connect **PIN1** and **PIN2** on **P5** connector and **PIN1** and **PIN2** on **P6** connector to read data from the conductivity cell.   - Connect **PIN1** and **PIN2** on **P5** connector and **PIN1** and **PIN2** on **P6** connector to read data from the conductivity cell.
   - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14)   - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14)
 +
 ===== Obtaining the Source Code ===== ===== Obtaining the Source Code =====
  
-We recommend not opening the project directly, but rather import it into CrossCore Embedded Studios and make a local copy in your workspace+There are two basic ways to program the ADICUP360 with the software for the CN0411. 
 +  - Dragging and Dropping the .Bin to the MBED drive 
 +  - Building, Compiling, and Debugging using CCES
  
-The source code and include files of the **ADuCM360_demo_cn0411** can be found here:+Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. 
 + 
 +Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. 
 + 
 +The software for the **ADuCM360_demo_cn0411** demo can be found here:
  
 <WRAP round 80% download> <WRAP round 80% download>
-\\ +Prebuilt CN0411 Bin File 
-CrossCore Embedded Studio Application Source Code+  * [[https://github.com/analogdevicesinc/EVAL-ADICUP360/releases/download/Release-1.0/ADuCM360_demo_cn0411.bin| ADuCM360_demo_cn0411.Bin]] 
-\\ +Complete CN0411 Source Files 
-\\ +  [[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_cn0411| ADuCM360_demo_cn0411 Source Code]] 
-[[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_cn0411| AduCM360_demo_cn0411 at Github]] +
- +
 </WRAP> </WRAP>
  
resources/eval/user-guides/eval-adicup360/reference_designs/demo_cn0411.txt · Last modified: 14 Mar 2021 10:12 by Zuedmar Arceo