This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0409 [14 Jan 2021 05:24] – use / interwiki links Robin Getz | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0409 [14 Mar 2021 10:09] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | ||
---|---|---|---|
Line 66: | Line 66: | ||
{{: | {{: | ||
- | ===== Obtaining the source code ===== | + | ===== Obtaining the Source Code ===== |
- | We recommend not opening | + | |
+ | There are two basic ways to program | ||
+ | - Dragging and Dropping the .Bin to the MBED drive | ||
+ | - Building, Compiling, and Debugging using CCES | ||
+ | |||
+ | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. | ||
+ | |||
+ | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | ||
+ | |||
+ | The software for the **ADuCM360_demo_cn0409** demo can be found here: | ||
- | The source code and include files of the ADuCM360_demo_cn0409 can be found on Github: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | \\ | + | Prebuilt CN0409 Bin File |
- | CrossCore Embedded Studio Application Source Code: | + | * [[https:// |
- | \\ | + | Complete CN0409 Source Files |
- | \\ | + | |
- | [[https:// | + | |
- | </ | + | |
+ | </ | ||
<WRAP center round info 80%> | <WRAP center round info 80%> | ||
For more information on importing, debugging, or other tools related questions, please see the [[/ | For more information on importing, debugging, or other tools related questions, please see the [[/ |