Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0397 [14 Jan 2021 05:24]
Robin Getz use / interwiki links
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0397 [14 Mar 2021 10:05]
Zuedmar Arceo [Obtaining the Source Code] adding in .Bin file
Line 55: Line 55:
   - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14)   - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14)
  
-===== Obtaining the source code =====+===== Obtaining the Source Code =====
  
-We recommend not opening ​the project directly, but rather import it into CCES and make a local copy in your workspace+There are two basic ways to program ​the ADICUP360 with the software for the CN0397. 
 +  - Dragging ​and Dropping the .Bin to the MBED drive 
 +  - Building, Compiling, and Debugging using CCES
  
-The source code and include files of the **ADuCM360_demo_cn0397** can be found on Github:+Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. 
 + 
 +Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. 
 + 
 +The software for the **ADuCM360_demo_cn0397** ​demo can be found here:
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-\\  +Prebuilt CN0397 Bin File 
-CrossCore Embedded Studio Application Source Code+  * [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP360/​releases/​download/​Release-1.0/​ADuCM360_demo_cn0397.bin| ADuCM360_demo_cn0397.Bin]] 
-\\  +Complete CN0397 Source Files 
-\\  +  ​* ​[[https://​github.com/​analogdevicesinc/​EVAL-ADICUP360/​tree/​master/​projects/​ADuCM360_demo_cn0397| ​ADuCM360_demo_cn0397 Source Code]]
-[[https://​github.com/​analogdevicesinc/​EVAL-ADICUP360/​tree/​master/​projects/​ADuCM360_demo_cn0397| ​AduCM360_demo_cn0397 at Github]] +
-</​WRAP>​+
  
 +</​WRAP>​
 <WRAP center round info 80%> <WRAP center round info 80%>
 For more information on importing, debugging, or other tools related questions, please see the [[/​resources/​eval/​user-guides/​eval-adicup360/​tools/​cces_user_guide |tools user guide.]] ​ For more information on importing, debugging, or other tools related questions, please see the [[/​resources/​eval/​user-guides/​eval-adicup360/​tools/​cces_user_guide |tools user guide.]] ​
resources/eval/user-guides/eval-adicup360/reference_designs/demo_cn0397.txt · Last modified: 14 Mar 2021 10:05 by Zuedmar Arceo