This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0394 [14 Jan 2021 05:24] – use / interwiki links Robin Getz | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0394 [14 Mar 2021 09:55] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | ||
---|---|---|---|
Line 92: | Line 92: | ||
- Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | ||
- | ===== Obtaining the source code ===== | + | ===== Obtaining the Source Code ===== |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the ADuCM360_demo_cn0394 can be found on Github: | + | Using the drag and drop method, |
- | <WRAP round download | + | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download |
- | \\ | + | |
- | CrossCore | + | |
- | \\ | + | |
- | \\ | + | |
- | [[https:// | + | |
- | </ | + | |
+ | The software for the **ADuCM360_demo_cn0394** demo can be found here: | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | Prebuilt CN0394 Bin File | ||
+ | * [[https:// | ||
+ | Complete CN0394 Source Files | ||
+ | * [[https:// | ||
+ | |||
+ | </ | ||
<WRAP center round info 80%> | <WRAP center round info 80%> | ||
For more information on importing, debugging, or other tools related questions, please see the [[/ | For more information on importing, debugging, or other tools related questions, please see the [[/ |