Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0391 [14 Jan 2021 05:24]
Robin Getz use / interwiki links
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0391 [14 Mar 2021 09:53]
Zuedmar Arceo [Obtaining the Source Code] adding in .Bin file
Line 90: Line 90:
  
  
-===== Obtaining the source code =====+===== Obtaining the Source Code =====
  
-We recommend not opening ​the project directly, but rather import it into CCES and make a local copy in your workspace.+There are two basic ways to program ​the ADICUP360 with the software for the CN0391. 
 +  - Dragging ​and Dropping the .Bin to the MBED drive 
 +  - Building, Compiling, and Debugging using CCES
  
-The source code and include files of the ADuCM360_demo_cn0391 can be found on Github+Using the drag and drop method, ​the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. 
 + 
 +Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. 
 + 
 +The software for the **ADuCM360_demo_cn0391** demo can be found here: 
 + 
 +<WRAP round 80% download>​ 
 +Prebuilt CN0391 Bin File 
 +  * [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP360/​releases/​download/​Release-1.0/​ADuCM360_demo_cn0391.bin| ADuCM360_demo_cn0391.Bin]] 
 +Complete CN0391 Source Files 
 +  * [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP360/​tree/​master/​projects/​ADuCM360_demo_cn0391| ADuCM360_demo_cn0391 Source Code]]
  
-<WRAP round download 80%> 
-\\  
-CrossCore Embedded Studio Application Source Code: 
-\\  
-\\  
-[[https://​github.com/​analogdevicesinc/​EVAL-ADICUP360/​tree/​master/​projects/​ADuCM360_demo_cn0391|ADuCM360_demo_cn0391]] 
 </​WRAP>​ </​WRAP>​
  
resources/eval/user-guides/eval-adicup360/reference_designs/demo_cn0391.txt · Last modified: 14 Mar 2021 09:53 by Zuedmar Arceo