This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0357 [14 Jan 2021 05:24] Robin Getz use / interwiki links |
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0357 [14 Mar 2021 09:51] Zuedmar Arceo [Obtaining the Source Code] adding in .Bin file |
||
---|---|---|---|
Line 56: | Line 56: | ||
- Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | ||
- | ===== Obtaining the source code ===== | + | ===== Obtaining the Source Code ===== |
+ | There are two basic ways to program the ADICUP360 with the software for the CN0357. | ||
+ | - Dragging and Dropping the .Bin to the MBED drive | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | We recommend not opening the project directly, but rather import it into CCES and make a local copy in your workspace. | + | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. |
- | The source code and include files of the **ADuCM360_demo_cn0357** can be found on Github: | + | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. |
+ | |||
+ | The software for the **ADuCM360_demo_cn0357** demo can be found here: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | \\ | + | Prebuilt CN0357 Bin File |
- | CrossCore Embedded Studio Application Source Code: | + | * [[https://github.com/analogdevicesinc/EVAL-ADICUP360/releases/download/Release-1.0/ADuCM360_demo_cn0357.bin| ADuCM360_demo_cn0357.Bin]] |
- | \\ | + | Complete CN0357 Source Files |
- | \\ | + | * [[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_cn0357| ADuCM360_demo_cn0357 Source Code]] |
- | [[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_cn0357| ADuCM360_demo_cn0357 at Github]] | + | |
- | </WRAP> | + | |
+ | </WRAP> | ||
<WRAP center round info 80%> | <WRAP center round info 80%> | ||
For more information on importing, debugging, or other tools related questions, please see the [[/resources/eval/user-guides/eval-adicup360/tools/cces_user_guide |tools user guide.]] | For more information on importing, debugging, or other tools related questions, please see the [[/resources/eval/user-guides/eval-adicup360/tools/cces_user_guide |tools user guide.]] |