This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0216 [12 Dec 2017 21:38] – Brandon Bushey | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0216 [16 Jan 2018 18:27] – Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======Weigh Scale Measurement Demo====== | + | ====== Weigh Scale Measurement Demo ====== |
- | The **ADuCM360_demo_cn0216** is a weigh scale measurement demo project for the EVAL-ADICUP360 base board with additional [[http:// | + | The **ADuCM360_demo_cn0216** is a weigh scale measurement demo project for the EVAL-ADICUP360 base board with additional [[http:// |
\\ | \\ | ||
Line 62: | Line 62: | ||
- Connect your weigh scale to the EVAL-CN0216-ARDZ via **()**, make sure you pay attention to the pinout which can be found on the [[https:// | - Connect your weigh scale to the EVAL-CN0216-ARDZ via **()**, make sure you pay attention to the pinout which can be found on the [[https:// | ||
- Connect an acceptable 7V-12V power supply into the P11 barrel jack of the EVAL-ADICUP360 | - Connect an acceptable 7V-12V power supply into the P11 barrel jack of the EVAL-ADICUP360 | ||
- | <note important> | + | <note important> |
- Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | ||