This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cli [14 Jan 2021 05:23] Robin Getz use / interwiki links |
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cli [14 Mar 2021 06:15] Zuedmar Arceo [Obtaining the Source Code] adding in .Bin file |
||
---|---|---|---|
Line 79: | Line 79: | ||
\\ | \\ | ||
- | ===== Obtaining the source code ===== | + | ===== Obtaining the Source Code ===== |
- | \\ | + | |
- | We recommend not opening the project directly, but rather import it into Eclipse and make a local copy in your Eclipse workspace. | + | There are two basic ways to program the ADICUP360 with the software for the CLI Demo. |
+ | - Dragging and Dropping the .Bin to the MBED drive | ||
+ | - Building, Compiling, and Debugging using CCES | ||
+ | |||
+ | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. | ||
+ | |||
+ | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | ||
+ | |||
+ | The software for the **ADuCM360_demo_cli** demo can be found here: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
+ | Prebuilt CLI Demo Bin File | ||
+ | * [[https://github.com/analogdevicesinc/EVAL-ADICUP360/releases/download/Release-1.0/ADuCM360_demo_cli.bin| ADuCM360_demo_cli.Bin]] | ||
+ | Complete CLI Demo Source Files | ||
+ | * [[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_cli| ADuCM360_demo_cli Source Code]] | ||
- | [[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_cli | ADuCM360_demo_cli at Github]] | ||
- | |||
</WRAP> | </WRAP> | ||