Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
resources:eval:user-guides:eval-adicup360:reference_designs:demo_adxl355 [14 Jan 2021 05:23] – use / interwiki links Robin Getzresources:eval:user-guides:eval-adicup360:reference_designs:demo_adxl355 [14 Mar 2021 05:54] – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo
Line 46: Line 46:
   - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the **User USB**.(P13)   - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the **User USB**.(P13)
  
-===== Obtaining the source code =====+===== Obtaining the Source Code =====
  
-We recommend not opening the project directly, but rather import it into CCES and make a local copy in your workspace+There are two basic ways to program the ADICUP360 with the software for the ADXL355. 
 +  - Dragging and Dropping the .Bin to the MBED drive 
 +  - Building, Compiling, and Debugging using CCES
  
-The source code and include files of the **ADuCM360_demo_adxl355_pmdz** can be found on Github:+Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. 
 + 
 +The software for the **ADuCM360_demo_adxl355** demo can be found here:
  
 <WRAP round 80% download> <WRAP round 80% download>
-\\  +Prebuilt ADXL355 Bin File 
-CrossCore Embedded Studio Application Source Code+  * [[https://github.com/analogdevicesinc/EVAL-ADICUP360/releases/download/Release-1.0/ADuCM360_demo_adxl355_pmdz.bin| AduCM3029_demo_adxl355_pmdz.Bin]] 
-\\  +Complete ADXL355 Source Files 
-\\  +  [[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_adxl355_pmdz| AduCM3029_demo_adxl355 Source Code]] 
-[[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_adxl355_pmdz| AduCM360_demo_adxl355_pmdz at Github]]+
 </WRAP> </WRAP>
 +
  
 <WRAP center round info 80%> <WRAP center round info 80%>
resources/eval/user-guides/eval-adicup360/reference_designs/demo_adxl355.txt · Last modified: 14 Mar 2021 06:10 by Zuedmar Arceo