The ADuCM360_demo_adxl355_pmdz is an accelerometer demo project for the EVAL-ADICUP360 base board with the EVAL-ADXL355-PMDZ board, using the GNU ARM Eclipse Plug-ins in Eclipse environment.
This project is an example for how to use EVAL-ADICUP360 board in combination with the EVAL-ADXL355-PMDZ accelerometer PMOD board.
The ADuCM360_demo_adxl355_pmdz project uses the EVAL-ADXL355-PMDZ which has the ADXL355 3-axis MEMS accelerometer on board.
The application reads the X , Y , and Z acceleration registers. The acceleration in the 3 axis is displayed in [G]. There is an internal temperature sensor in the ADXL355, which is converted by the on chip 12-bit ADC. The acceleration range can also be selected by setting the ADXL355_RANGE variable with the ADXL355.h file. (Values of [2, 4, and 8 are acceptable] )
All the outputs are printed from the UART to the USER USB port and can be read on the PC using a serial terminal program, such as Putty or Tera Term.
For precision applications, each ADXL355 chip requires individual calibration which can be done by measuring and setting the definitions ACC_TEMP_BIAS and ACC_TEMP_SENSITIVITY parameters in the ADXL362.h file.
The temperature in degrees celsius, can be derived from the ADC readings Tadc using the predefined formula:
Temp = (Tadc - ADXL355_TEMP_BIAS)/ ADXL355_TEMP_SLOPE) + 25;
The following is a list of items needed in order to replicate this demo.
There are two basic ways to program the ADICUP360 with the software for the ADXL355.
Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design.
Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain.
The software for the ADuCM360_demo_adxl355 demo can be found here:
Prebuilt ADXL355 Bin File
Complete ADXL355 Source Files
For more information on importing, debugging, or other tools related questions, please see the tools user guide.
#define ADXL355_TEMP_BIAS (float)1852.0 #define ADXL355_TEMP_SLOPE (float)-9.05
#define ADXL_SENSE 2
#define ACT_VALUE 50 #define INACT_VALUE 50
#define ACT_TIMER 50 #define INACT_TIMER 50
Following is the UART configuration.
Select COM Port Baud rate: 9600 Data: 8 bit Parity: none Stop: 1 bit Flow Control: none
The user must press the <ENTER> key each time they want to display the results.
The official tool we promote for use with the EVAL-ADICUP360 is CrossCore Embedded Studio. For more information on downloading the tools and a quick start guide on how to use the tool basics, please check out the Tools Overview page.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to import existing projects into your workspace section.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to configure the debug session section.
The ADuCM360_demo_adxl355_pmdz project use basic ARM Cortex-M C/C++ Project structure.
This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripheral; port configuration for SPI0, accelerometer sensor use; SPI read/write functions; sensor monitoring.
In the src and include folders you will find the source and header files related to ADXL355 application. You can modify as you wanted those files. The Communication.c/h files contain SPI and UART specific data, meanwhile the ADXL355.c/h files contain the accelerometer data. Here are parameters you can configure:
The RTE folder contains device and system related files:
End of Document