This is an old revision of the document!
The ADuCM360_demo_adt7420_pmdz is a temperature demo project for the EVAL-ADICUP360 base board with an EVAL-ADT7420-PMDZ PMOD board from Analog Devices, using the GNU ARM Eclipse Plug-ins in Eclipse environment.
This project is an example for how to use EVAL-ADICUP360 board in combination with the EVAL-ADT7420-PMDZ Temperature PMOD.
The ADuCM360_demo_adt7420_pmdz project uses the EVAL-ADT7420-PMDZ which has the ADT7420 0.25 degree accurate digital temperature sensor on board.
The application reads the temperature data from the ADT7420 and displays the temperature in [codes] and [C] on a serial terminal. The temperature data can be changed between 16-bit(0.0078 C/LSB) and 13-bit(0.0625 C/LSB) accurate depending on the resolution needed. The application also prints out the device ID register, which is just a quick and easy check to ensure the reads are working properly.
All the outputs are printed from the UART to the USER USB port using P0.6 and P0.7, and can be read on the PC using a serial terminal program, such as Putty or Tera Term. The user must ensure that the USB cable is connected to the USER USB port in order to read back values in Putty. Also, the user must press the <ENTER> key in order to refresh the results.
We recommend not opening the project directly, but rather import it into Eclipse and make a local copy in your Eclipse workspace.
To learn how to import the ADuCM360_demo_adt7420_pmdz project form the projects examples in the Git repository, please click on How to import existing projects from the GIT Repository.
The source code and include files of the ADuCM360_demo_adt7420_pmdz can be found on Github:
The necessary instructions on how to import ADuCM360_demo_adt7420_pmdz project in your workspace can be found in the section, Import a project into workspace.
After completion of the steps above the program will remain written into the system flash and it will run by default every time the board is powered up.
The ADuCM360_demo_adt7420_pmdz project use basic ARM Cortex-M C/C++ Project structure.
This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripheral; port configuration for I2C, temperature sensor data; I2C read/write functions; threshold monitoring.
In the src and include folders you will find the source and header files related to adt7420_pmdz application. You can modify those files as appropriate for your application. The Communication.c/h files contain I2C and UART specific data, meanwhile the ADT7420.c/h files contain the temperature information data and threshold registers. Here are parameters you can configure:
uint8_t ui8configAdt7420 = (FAULT_TRIGGER_4 | CT_PIN_POLARITY | INT_PIN_POLARITY | INT_CT_MODE |CONTINUOUS_CONVERSION_MODE | RESOLUTION_13_BITS); /** #define FAULT_TRIGGER_1 - 1 fault reading triggers an interrupt #define FAULT_TRIGGER_2 - 2 fault readings triggers an interrupt #define FAULT_TRIGGER_3 - 3 fault readings triggers an interrupt #define FAULT_TRIGGER_4 - 4 fault readings triggers an interrupt #define CT_PIN_POLARITY - Critical temp active logic level #define INT_PIN_POLARITY - Interrupt temp active logic level #define INT_CT_MODE - Selects comparator or interrupt mode #define CONTINUOUS_CONVERSION_MODE - Continuous conversion #define ONE_SHOT_MODE - One shot conversion, then shuts down #define ONE_SAMPLE_PER_SECOND_MODE - One second between readings #define SHUTDOWN_MODE - Power down mode activated #define RESOLUTION_13_BITS - 13-bit Temperature data #define RESOLUTION_16_BITS - 16-bit Temperature data **/
#define ADT7420_ADDRESS 0x48
#define TEMP_HIGH_SETPOINT 75
#define TEMP_LOW_SETPOINT 0
#define TEMP_CRITICAL_SETPOINT 100
#define TEMP_HYSTERSIS_SETPOINT 5
The system folder contains system related files (try not to change these files):