Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [06 Oct 2017 22:29]
Brandon reordering and adding sections
resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [12 Dec 2017 21:34]
Brandon
Line 34: Line 34:
  
 ===== Setting up the hardware ===== ===== Setting up the hardware =====
-\\ 
  
- - To program the base board, set the jumpers as shown in the next figure. The important jumpers are highlighted in red.{{ :​resources:​eval:​user-guides:​eval-adicup360:​reference_designs:​adt7420:​aduicup360_switch_config.png?​500 |}}+ - To program the base board, set the jumpers/​switches ​as shown in the next figure. The important jumpers/​switches ​are highlighted in red.{{ :​resources:​eval:​user-guides:​eval-adicup360:​reference_designs:​adt7420:​aduicup360_switch_config.png?​500 |}}
  - Plug the EVAL-ADT7420-PMDZ PMOD in the EVAL-ADICUP360 base board, via the PMOD_I2C port (P10).  - Plug the EVAL-ADT7420-PMDZ PMOD in the EVAL-ADICUP360 base board, via the PMOD_I2C port (P10).
-Power EVAL-ADICUP360 base board via the Debug USB.+Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14)
  
-\\ 
 ===== Obtaining the source code ===== ===== Obtaining the source code =====
-\\ 
  
-We recommend not opening the project directly, but rather import it into Eclipse ​and make a local copy in your Eclipse ​workspace. ​+We recommend not opening the project directly, but rather import it into CCES and make a local copy in your workspace. ​
  
 The source code and include files of the **ADuCM360_demo_adt7420_pmdz** can be found on Github: The source code and include files of the **ADuCM360_demo_adt7420_pmdz** can be found on Github:
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
 +\\  
 +CrossCore Embedded Studio Application Source Code: 
 +\\  
 +\\ 
 [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP360/​tree/​master/​projects/​ADuCM360_demo_adt7420_pmdz| AduCM360_demo_adt7420_pmdz at Github]] [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP360/​tree/​master/​projects/​ADuCM360_demo_adt7420_pmdz| AduCM360_demo_adt7420_pmdz at Github]]
-  
 </​WRAP>​ </​WRAP>​
 +
  
 <WRAP center round info 80%> <WRAP center round info 80%>
Line 58: Line 58:
 </​WRAP>​ </​WRAP>​
  
-\\ 
 ===== Configuring the Software Parameters ===== ===== Configuring the Software Parameters =====
  
Line 114: Line 113:
  
 ==== Serial Terminal Output ==== ==== Serial Terminal Output ====
 +
 +  - In order to view the data, you must flash the program to the EVAL-ADICUP360.  ​
 +  - Once complete you will need to switch the USB cable from the DEBUG USB (P14) to the USER USB (P13).  ​
 +  - Then follow the UART settings below with the serial terminal program.
 +\\ 
  
 Following is the UART configuration. Following is the UART configuration.
Line 134: Line 138:
 ==== Importing ==== ==== Importing ====
  
-For more detailed instructions on importing this application/​demo example into the CrossCore Embedded Studios tools, please view our [[resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide#​how_to_import_existing_projects_into_your_workspace|How to import existing projects into your workspace]] section.+For more detailed instructions on importing this application/​demo example into the CrossCore Embedded Studios tools, please view our [[resources:​eval:​user-guides:​eval-adicup360:​tools:​cces_user_guide#​how_to_import_existing_projects_into_your_workspace|How to import existing projects into your workspace]] section.
  
 ==== Debugging ==== ==== Debugging ====
  
-For more detailed instructions on importing this application/​demo example into the CrossCore Embedded Studios tools, please view our [[resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide#​how_to_configure_the_debug_session_for_an_aducm3029_application|How to configure the debug session]] section.+For more detailed instructions on importing this application/​demo example into the CrossCore Embedded Studios tools, please view our [[resources:​eval:​user-guides:​eval-adicup360:​tools:​cces_user_guide#​how_to_configure_the_debug_session_for_an_aducm360_application|How to configure the debug session]] section.
  
 ==== Project Structure ==== ==== Project Structure ====
resources/eval/user-guides/eval-adicup360/reference_designs/demo_adt7420.txt · Last modified: 12 Dec 2017 21:34 by Brandon