This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [06 Oct 2017 22:29] – reordering and adding sections Brandon Bushey | resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [20 Oct 2017 21:28] – Brandon Bushey | ||
---|---|---|---|
Line 34: | Line 34: | ||
===== Setting up the hardware ===== | ===== Setting up the hardware ===== | ||
- | \\ | ||
- | - To program the base board, set the jumpers as shown in the next figure. The important jumpers are highlighted in red.{{ : | + | - To program the base board, set the jumpers/ |
- Plug the EVAL-ADT7420-PMDZ PMOD in the EVAL-ADICUP360 base board, via the PMOD_I2C port (P10). | - Plug the EVAL-ADT7420-PMDZ PMOD in the EVAL-ADICUP360 base board, via the PMOD_I2C port (P10). | ||
- | - Power EVAL-ADICUP360 base board via the Debug USB. | + | - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) |
- | \\ | ||
===== Obtaining the source code ===== | ===== Obtaining the source code ===== | ||
- | \\ | ||
- | We recommend not opening the project directly, but rather import it into Eclipse | + | We recommend not opening the project directly, but rather import it into CCES and make a local copy in your workspace. |
The source code and include files of the **ADuCM360_demo_adt7420_pmdz** can be found on Github: | The source code and include files of the **ADuCM360_demo_adt7420_pmdz** can be found on Github: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | + | [[https:// | |
- | [[https:// | + | |
- | + | ||
</ | </ | ||
Line 58: | Line 53: | ||
</ | </ | ||
- | \\ | ||
===== Configuring the Software Parameters ===== | ===== Configuring the Software Parameters ===== | ||
Line 114: | Line 108: | ||
==== Serial Terminal Output ==== | ==== Serial Terminal Output ==== | ||
+ | |||
+ | - In order to view the data, you must flash the program to the EVAL-ADICUP360. | ||
+ | - Once complete you will need to switch the USB cable from the DEBUG USB (P14) to the USER USB (P13). | ||
+ | - Then follow the UART settings below with the serial terminal program. | ||
+ | \\ | ||
Following is the UART configuration. | Following is the UART configuration. | ||
Line 134: | Line 133: | ||
==== Importing ==== | ==== Importing ==== | ||
- | For more detailed instructions on importing this application/ | + | For more detailed instructions on importing this application/ |
==== Debugging ==== | ==== Debugging ==== | ||
- | For more detailed instructions on importing this application/ | + | For more detailed instructions on importing this application/ |
==== Project Structure ==== | ==== Project Structure ==== |