Wiki

This version (01 Mar 2018 18:21) was approved by Brandon Bushey.The Previously approved version (01 Mar 2018 18:20) is available.Diff

Hardware Cases and Enclosures

3D Printer Cases

There are enclosures made for the EVAL-ADICUP360 and attachable daughter boards. I have put together a table of the current 3D printable cases we have to date. If you have created a 3D case for the ADICUP360 and would like to have it added to this table, please do so. We will review your submission and work on adding it to the list.

If you would like to view the designs in a 3D environment to get a better idea of what the design looks like, there are many free STL viewers that exist on the internet. I've provided a link below to the one that I think is the easiest to use, you can simply drag and drop the STL files into the browser.

http://www.viewstl.com/

These 3D printer STL files were made by community contributors as additional collateral to the ADICUP360 ecosystem. Analog Devices is NOT responsible for 3D files that print incorrectly or are not compatible with your particular printer. It is up to the user to make sure the enclosures can be printed on their machines.

3D STL File Boards Intended for Case Description Picture
ADICUP360 Case 1 EVAL-ADICUP360 * Base plate used for ADICUP360 board and add on boards.
* Screw holes lined up for secure installation
resources/eval/user-guides/eval-adicup360/mechanical.txt · Last modified: 01 Mar 2018 18:21 by Brandon Bushey