Wiki

This version is outdated by a newer approved version.DiffThis version (05 Apr 2021 18:39) was approved by Brandon Bushey.The Previously approved version (03 Jan 2021 21:46) is available.Diff

This is an old revision of the document!


EVAL-CN0396-ARDZ Shield - Hardware User Guide

CN0396 is single-supply, low noise, portable gas detector, using a 4-electrode electrochemical sensor, for simultaneous detection of two distinct gases. The Alphasense COH-A2 sensor, which detects carbon monoxide(CO) and hydrogen sulfide(H2S), is used in this example. Electrochemical sensors offer several advantages for instruments that detect or measure the concentration of many toxic gases. Most sensors are gas specific and have usable resolutions under one part per million (ppm) of gas concentration.

The circuit shown in below uses the ADA4528-2, dual auto zero amplifier, which has a maximum offset voltage of 2.5 µV at room temperature and an industry leading 5.6 µV/√Hz of voltage noise density. In addition, the AD5270-20 programmable rheostat is used rather than a fixed transimpedance resistor, allowing for rapid prototyping of different gas sensor systems, without changing the bill of materials. The ADR3412 precision, low noise, micropower reference establishes the 1.2 V common-mode, pseudo ground reference voltage with 0.1% accuracy and 8 ppm/°C drift. For applications where measuring fractions of ppm gas concentration is important, using the ADA4528-2 and the ADR3412 makes the circuit performance suitable for interfacing with a 16-bit ADC, such as the AD7790.

An ADT7310 16-Bit Digital SPI Temperature Sensor is also included in the circuit to allow for monitoring of environmental temp. This allows for correction of the temperature effects on the sensor.

The EVAL-CN0396-ARDZ Shield is designed to be compatible with the Arduino R3 shield form factor. It is compatible with either 5V or 3.3V processor boards.



Equipment Needed

Hardware

  • EVAL-CN0396-ARDZ Circuit Evaluation Board
  • EVAL-ADICUP360 Development Board / Arduino R3 compatible processor Board
  • Power supply: 6 V or 6 V wall wart (not needed if plugged into the PC via USB)
  • 4-Electrode Electrochemical Gas Sensor (CO-H2S sensor is provided with the evaluation board)
  • Environmental chamber
  • Calibration Gases
  • Precision Current Sources (alternative to actual sensor and gases)

Software - using ADICUP360

  • PC with a USB port and Windows 7 (32-bit) or higher
  • ADICUP360 Eclipse IDE
  • CN0396 Demo Software
  • Serial Terminal Software (Putty/TeraTerm or similar)

Hardware Setup

  • Connect the EVAL-CN0396-ARDZ board to the microprocessor boards using mating headers POWER, ANALOG, DIGI0, DIGI1 and ICSP
  • Connect your 4-Electrode Electrochemical Gas Sensor to socket M1
  • The EVAL-CN0396-ARDZ board is powered by the POWER header when using an Arduino form factor compatible processor board. Ensure that 5V(ANALOG - Pin 5), IOREF(ANALOG - Pin 2) and GND(ANALOG - Pin 6/7) pins are connected.

Connectors, Sensors, and Configurations


Gas Sensors

The evaluation board comes packaged with an Alphasense COH-A2 sensor. Sockets are already provided for easy installation of the sensor.

Pin Compatible Sensors:

Sensor Socket Connection

Pin Name Description
WE1 Working Electrode (CO gas electrode for COH-A2 sensor)
CE Counter Electrode
WE2 Working Electrode (H2S gas electrode for COH-A2 sensor)
RE Reference Electrode

Note: Not all sensors provided in this list have been tested with the EVAL-CN0396-ARDZ. Using different sensors may require modifications to the Software and/or the Hardware.


Chip Select

There are three(3) headers on the board allow for selection of the digital pin to be used as the Chip Select (CS) signal for the AD7798, AD5270 and ADT7310 SPI digital communications.

  • AD7798_CS - selects either Arduino Pin D9 or D10 as CS for AD7798 ADC.
AD7798_CS Connections Arduino Pin
Jumper Pin 1 and Pin 2 D10
Jumper Pin 2 and Pin 3 D9
  • AD5270_CS - selects either Arduino Pin D5 or D6 as CS for AD5270 Digital Rheostat
AD5270_CS Connections Arduino Pin
Jumper Pin 1 and Pin 2 D6
Jumper Pin 2 and Pin 3 D5
  • ADT7310_CS - selects either Arduino Pin D3 or D4 as CS for ADT7310 Digital Temp Sensor
ADT7310_CS Connections Arduino Pin
Jumper Pin 1 and Pin 2 D4
Jumper Pin 2 and Pin 3 D3

Schematic, PCB Layout, Bill of Materials

EVAL-CN0396-ARDZ Design & Integration Files

  • Schematics
  • PCB Layout
  • Bill of Materials
  • Allegro Project

Software

resources/eval/user-guides/eval-adicup360/hardware/cn0396.1617640731.txt.gz · Last modified: 05 Apr 2021 18:38 by Brandon Bushey