This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:hardware:cn0391 [27 Oct 2016 16:07] – [Connectors and Jumper Configurations] adding CS jumper Brandon Bushey | resources:eval:user-guides:eval-adicup360:hardware:cn0391 [29 Jul 2021 05:16] (current) – [Registration] Zuedmar Arceo | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== EVAL-CN0391-ARDZ Shield ====== | + | ====== EVAL-CN0391-ARDZ Shield ====== |
- | The [[http:// | + | ===== Overview ===== |
+ | |||
+ | The [[adi>cn0391|EVAL-CN0391-ARDZ shield]] is a single supply, multi channel thermocouple temperature meter. The CN0391 uses [[adi>ad7124-8|AD7124-8]] 8-Channel, Low Noise, Low Power, 24-Bit, Sigma-Delta ADC with PGA and Reference as integrated solution for multi channel thermocouple temperature measurement with RTD cold junction compensation. | ||
{{ : | {{ : | ||
Line 8: | Line 10: | ||
* EVAL-CN0391-ARDZ Circuit Evaluation Board | * EVAL-CN0391-ARDZ Circuit Evaluation Board | ||
- | * [[http:// | + | * [[adi>EVAL-ADICUP360|EVAL-ADICUP360]] Development Board or compatible Arduino platform Board. |
* Any combination of B, E, J, K, N, R, S, T type thermocouples (total of 4) | * Any combination of B, E, J, K, N, R, S, T type thermocouples (total of 4) | ||
* PC with Microsoft Windows 7 64-bit or later and USB 2.0 port or higher | * PC with Microsoft Windows 7 64-bit or later and USB 2.0 port or higher | ||
Line 20: | Line 22: | ||
* Connect the EVAL-ADICUP360 **USER** USB port to PC with USB cable | * Connect the EVAL-ADICUP360 **USER** USB port to PC with USB cable | ||
- | ====== Connectors and Jumper Configurations ====== | + | ===== Connectors and Jumper Configurations ===== |
+ | |||
+ | ==== Thermocouple Connectors | ||
Each of the four(4) channels uses an Omega style connector for the thermocouples, | Each of the four(4) channels uses an Omega style connector for the thermocouples, | ||
+ | |||
+ | There is an RTD beneath the copper tabs of each connector which is used to measure the cold junction temperature. | ||
==== Chip Select ==== | ==== Chip Select ==== | ||
Line 36: | Line 42: | ||
{{ : | {{ : | ||
| | ||
- | ====== Schematic, PCB Layout, Bill of Materials ====== | + | ===== Digital Communications ===== |
+ | |||
+ | The AD7124 Analog to Digital converter, measures each sensor input channel on the board. | ||
+ | |||
+ | The SPI digital communications lines can be found on two(2) connectors on the EVAL-CN0391-ARDZ. | ||
+ | P8 and P7 have the SPI lines to handle the communication between the AD7124 and the processor. | ||
+ | |||
+ | ==== SPI Connectors (P8 & P7) ==== | ||
+ | |||
+ | ^ P8 Connector Pins ^ SPI Function ^ | ||
+ | | Pin 1,2, or 3 | SPI_CS | | ||
+ | | Pin 4 | SPI_MOSI | | ||
+ | | Pin 5 | SPI_MISO | | ||
+ | | Pin 6 | SPI_CLK | | ||
+ | |||
+ | ^ P7 Connector Pins ^ SPI Function ^ | ||
+ | | Pin 1 | SPI_MISO | | ||
+ | | Pin 3 | SPI_CLK | | ||
+ | | Pin 4 | SPI_MOSI | | ||
+ | < | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
Line 46: | Line 74: | ||
</ | </ | ||
- | ====== Software | + | ===== Software ===== |
- | * [[resources: | + | |
- | | + | * [[resources: |
- | | + | * [[resources:eval:user-guides: |
- | | + | |
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
- | {{navigation EVAL-ADICUP360# | + | //End of Document// |