This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:hardware:cn0391 [10 Oct 2016 11:17] – Robert Lee | resources:eval:user-guides:eval-adicup360:hardware:cn0391 [29 Jul 2021 05:16] (current) – [Registration] Zuedmar Arceo | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== EVAL-CN0391-ARDZ Shield ====== | + | ====== EVAL-CN0391-ARDZ Shield ====== |
- | The [[http:// | + | ===== Overview ===== |
- | //< | + | The [[adi>cn0391|EVAL-CN0391-ARDZ shield]] is a single supply, multi channel thermocouple temperature meter. The CN0391 uses [[adi> |
+ | |||
+ | {{ : | ||
===== Equipment Needed ===== | ===== Equipment Needed ===== | ||
* EVAL-CN0391-ARDZ Circuit Evaluation Board | * EVAL-CN0391-ARDZ Circuit Evaluation Board | ||
- | * [[http:// | + | * [[adi>EVAL-ADICUP360|EVAL-ADICUP360]] Development Board or compatible Arduino platform Board. |
- | * B, | + | * Any combination of B, E, J, K, N, R, S, T type thermocouples |
- | * PC with Microsoft Windows 7 64bit or later and USB2.0 port or higher | + | * PC with Microsoft Windows 7 64-bit |
- | * Serial terminal software | + | * Serial terminal software |
+ | * Such as Putty or Tera Term | ||
===== General Setup ===== | ===== General Setup ===== | ||
* Connect the EVAL-CN0391-ARDZ to EVAL-ADICUP360 board | * Connect the EVAL-CN0391-ARDZ to EVAL-ADICUP360 board | ||
- | * Connect 4 thermocouples to EVAL-CN0391-ARDZ **P1~P4** | + | * Connect 4 thermocouples to EVAL-CN0391-ARDZ **P1~P4**, marked on PCB with **CH0~CH3** |
* Connect the EVAL-ADICUP360 **USER** USB port to PC with USB cable | * Connect the EVAL-ADICUP360 **USER** USB port to PC with USB cable | ||
- | ====== Connectors and Jumper Configurations | + | ===== Connectors and Jumper Configurations ===== |
- | //picture// | + | ==== Thermocouple Connectors ==== |
+ | |||
+ | Each of the four(4) channels uses an Omega style connector for the thermocouples, | ||
+ | |||
+ | There is an RTD beneath the copper tabs of each connector which is used to measure the cold junction temperature. | ||
+ | |||
+ | ==== Chip Select ==== | ||
+ | |||
+ | The chip select header (JP1) is used to select the chip select pin on the AD7124. | ||
+ | ^ Jumper Position (JP1) ^ AD7124 Chip Select Pin (P8)^ | ||
+ | | Across Pin 1 and 2 | Pin 3 | | ||
+ | | Across Pin 3 and 4 | Pin 2 | | ||
+ | | Across Pin 5 and 6 | Pin 1 | | ||
+ | |||
+ | To use the EVAL-CN0391-ARDZ with the software we provide, please connect the thermocouples to each channel and set the software to corresponding thermocouple type/channel . Please set the default jumper position as pictured: | ||
+ | |||
+ | {{ : | ||
| | ||
- | ===== Chip Select | + | ===== Digital Communications |
- | | + | |
- | ====== Schematic, PCB Layout, Bill of Materials ====== | + | The AD7124 Analog to Digital converter, measures each sensor input channel on the board. |
+ | |||
+ | The SPI digital communications lines can be found on two(2) connectors on the EVAL-CN0391-ARDZ. | ||
+ | P8 and P7 have the SPI lines to handle the communication between the AD7124 and the processor. | ||
+ | |||
+ | ==== SPI Connectors (P8 & P7) ==== | ||
+ | |||
+ | ^ P8 Connector Pins ^ SPI Function ^ | ||
+ | | Pin 1,2, or 3 | SPI_CS | | ||
+ | | Pin 4 | SPI_MOSI | | ||
+ | | Pin 5 | SPI_MISO | | ||
+ | | Pin 6 | SPI_CLK | | ||
+ | |||
+ | ^ P7 Connector Pins ^ SPI Function ^ | ||
+ | | Pin 1 | SPI_MISO | | ||
+ | | Pin 3 | SPI_CLK | | ||
+ | | Pin 4 | SPI_MOSI | | ||
+ | < | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[www.analog.com/ | + | EVAL-CN0391-ARDZ Design & Integration Files |
- | * Schematics | + | * {{: |
- | * PCB Layout | + | * {{: |
- | * Bill of Materials | + | * {{: |
- | * Allegro Project | + | * {{: |
+ | </ | ||
+ | |||
+ | ===== Software ===== | ||
+ | |||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
</ | </ | ||
- | ====== Software ====== | ||
- | * [[resources: | ||
- | * AduCM360 Example Code | ||
- | * [[https:// | ||
- | |||
- | {{navigation EVAL-ADICUP360# | + | //End of Document// |