CN0357 single-supply, low noise, portable gas detector circuit using an electrochemical sensor. The Alphasense CO-AX carbon monoxide sensor is used in this example. Electrochemical sensors offer several advantages for instruments that detect or measure the concentration of many toxic gases. Most sensors are gas specific and have usable resolutions under one part per million (ppm) of gas concentration.
The circuit shown in below uses the ADA4528-2, dual auto zero amplifier, which has a maximum offset voltage of 2.5 µV at room temperature and an industry leading 5.6 µV/√Hz of voltage noise density. In addition, the AD5270-20 programmable rheostat is used rather than a fixed transimpedance resistor, allowing for rapid prototyping of different gas sensor systems, without changing the bill of materials.
The ADR3412 precision, low noise, micropower reference establishes the 1.2 V common-mode, pseudo ground reference voltage with 0.1% accuracy and 8 ppm/°C drift.
For applications where measuring fractions of ppm gas concentration is important, using the ADA4528-2 and the ADR3412 makes the circuit performance suitable for interfacing with a 16-bit ADC, such as the AD7790.
NOTE - Three electrode electrochemical toxic gas sensors can be used with the EVAL-CN0357-ARDZ The footprint can accommodate 3 different sizes of sensors.
The Alphasense CO-AX electrochemical gas sensor was used during testing and programming.
Recommended PCB Sockets(for Alphasense Sensors)
Jumper P1 Settings
This set of jumpers allows for changing the pin mapping of the AD7790 and AD5270 chip select lines to different Arduino digital pins. Place jumper/shunt as shown to connect to the corresponding Digital IO pin.
AD7790 CS Selection
Pin 1 shunted to Pin 2
CS connected to Digital Pin 10
Pin 3 shunted to Pin 4
CS connected to Digital Pin 9
Pin 5 shunted to Pin 6
CS connected to Digital Pin 8
AD5270 CS Selection
Pin 1 shunted to Pin 2
CS connected to Digital Pin 7
Pin 3 shunted to Pin 4
CS connected to Digital Pin 6
Pin 5 shunted to Pin 6
CS connected to Digital Pin 5
EVAL-CN0357-ARDZ Rev C Files
EVAL-CN0357-ARDZ Rev B Files
RevB to RevC:
End of Document