Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:eval-adicup360:hardware:cn0326 [19 May 2017 03:13]
erbe reyta [Sensor Probe Requirements]
resources:eval:user-guides:eval-adicup360:hardware:cn0326 [24 May 2017 19:49]
Brandon Bushey
Line 17: Line 17:
 ==== Sensor Probe Requirements ==== ==== Sensor Probe Requirements ====
  
-When using the CN0326 PMOD board, a general purpose pH probe with BNC connecter ​can be used for pH measurement. ​ An example of a pH probe that can be used is a product from [[https://​www.atlas-scientific.com/​product_pages/​probes/​ph_probe.html|Atlas]] or from [[https://​www.hach.com/​radiometer-probes/​radiometer-analytical-probes/​family?​productCategoryId=35547627768|Hach]]. ​ For temperature compensation,​ an RTD  sensor with RCA connector can be used.  An example is from [[https://​www.atlas-scientific.com/​product_pages/​probes/​pt1000.html|Atlas]] or from [[http://​sea.omega.com/​ph/​subsection/​rtd-elements-with-lead-wires-attached.html|Omega]]. ​ These sensors are required in order to run and capture analog signal from a sample solution and the connections can be seen on the diagram as shown below. ​  +When using the CN0326 PMOD board, a general purpose pH probe with BNC connector ​can be used for pH measurement. ​ An example of a pH probe that can be used is a product from [[https://​www.atlas-scientific.com/​product_pages/​probes/​ph_probe.html|Atlas]] or from [[https://​www.hach.com/​radiometer-probes/​radiometer-analytical-probes/​family?​productCategoryId=35547627768|Hach]]. ​ For temperature compensation,​ an RTD  sensor with RCA connector can be used.  An example is from [[https://​www.atlas-scientific.com/​product_pages/​probes/​pt1000.html|Atlas]] or from [[http://​sea.omega.com/​ph/​subsection/​rtd-elements-with-lead-wires-attached.html|Omega]]. ​ These sensors are required in order to run and capture analog signal from a sample solution and the connections can be seen on the diagram as shown below. ​  
  
 {{ :​resources:​eval:​user-guides:​eval-adicup360:​hardware:​cn0326:​sensor_interface.jpg |}} {{ :​resources:​eval:​user-guides:​eval-adicup360:​hardware:​cn0326:​sensor_interface.jpg |}}
Line 45: Line 45:
 ===== Software examples ===== ===== Software examples =====
  
-  * [[resources:​eval:​user-guides:​eval-adicup360:​reference_designs:​demo_cn0326|CN0326 Demo]]+  * [[resources:​eval:​user-guides:​eval-adicup360:​reference_designs:​demo_cn0326|ADICUP360 + CN0326 Demo]] 
 +  * [[resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​demo_cn0326|ADICUP3029 + CN0326 Demo]]
  
 ===== Schematics, PCB Layout, Bill of Materials ===== ===== Schematics, PCB Layout, Bill of Materials =====
Line 56: Line 57:
  
 </​WRAP>​ </​WRAP>​
 +
 +// End of Document //
resources/eval/user-guides/eval-adicup360/hardware/cn0326.txt · Last modified: 24 May 2017 19:49 by Brandon Bushey