Wiki

This version (17 Jul 2017 21:08) was approved by Brandon Bushey.The Previously approved version (04 Jan 2016 16:59) is available.Diff

ADICUP360 Compliance Results

Introduction

Regulatory compliance means conforming to a rule, such as a specification, policy, standard or law. Most products that ships into a country need to pass a variety of tests and regulations specific to that country.

Due to the increasing number of regulations, organizations are increasingly adopting the use of consolidated sets of compliance controls. This means once you normally get one, you can have them all.

Reports

The ADICUP360 passes all requirements of the CE tests.

What are all these logos?


All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.

Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.

resources/eval/user-guides/eval-adicup360/compliance_testing_and_results.txt · Last modified: 17 Jul 2017 21:08 by Brandon Bushey