Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:eval-adicup360:application_demos:smart_greenhouse [28 Jan 2021 17:35] – Fixed bad link for digikeys Ioana Chelaruresources:eval:user-guides:eval-adicup360:application_demos:smart_greenhouse [14 Mar 2021 10:15] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo
Line 82: Line 82:
 The software allows calibration of the pH sensors and the photodiodes on the board for more accurate measurements. The LED's can be controlled manually using the software and automatically by setting the desired intensity of each wavelength and using proportional control. The software allows calibration of the pH sensors and the photodiodes on the board for more accurate measurements. The LED's can be controlled manually using the software and automatically by setting the desired intensity of each wavelength and using proportional control.
  
-===== Obtaining the source code ===== +===== Obtaining the Source Code =====
-\\+
  
-We recommend not opening the project directly, but rather import it into Eclipse and make a local copy in your Eclipse workspace+There are two basic ways to program the ADICUP360 with the software for the Smart Greenhouse Demo. 
 +  - Dragging and Dropping the .Bin to the MBED drive 
 +  - Building, Compiling, and Debugging using CCES
  
-The source code and include files of the **ADuCM360_demo_Smart_Greenhouse** can be found on Github:+Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. 
 + 
 +Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. 
 + 
 +The software for the **ADuCM360_demo_Smart_Greenhouse** demo can be found here:
  
 <WRAP round 80% download> <WRAP round 80% download>
-\\  +Prebuilt Smart Greenhouse Demo Bin File 
-CrossCore Embedded Studio Application Source Code+  * [[https://github.com/analogdevicesinc/EVAL-ADICUP360/releases/download/Release-1.0/ADuCM360_demo_Smart_Greenhouse.bin| ADuCM360_demo_Smart_Greenhouse.Bin]] 
-\\  +Complete Smart Greenhouse Demo Source Files 
-\\  +  [[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_Smart_Greenhouse| ADuCM360_demo_Smart_Greenhouse Source Code]] 
-[[https://github.com/analogdevicesinc/EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_Smart_Greenhouse| ADuCM360_demo_Smart_Greenhouse]]+
 </WRAP> </WRAP>
  
resources/eval/user-guides/eval-adicup360/application_demos/smart_greenhouse.txt · Last modified: 14 Mar 2021 10:15 by Zuedmar Arceo