This is an old revision of the document!
CrossCore Embedded Studio Quickstart User Guide
This page describes how to use the ADuCM302x Device Family Pack (DFP) with CrossCore Embedded Studio (CCES) to create, import, build and debug applications for the ADuCM302x processor. The ADuCM302x processor integrates an ARM Cortex-M3 microcontroller with various on-chip peripherals within a single package.
This page describes how to install and work with the Analog Devices ADuCM302x DFP to start developing applications for the EVAL-ADICUP3029. This page also highlights common problems and how to avoid them.
Additional help documentation can be found by opening CCES and selecting “Help Contents” from the CCES Help menu.
This page covers:
How to install or upgrade the ADuCM302x Device Family Pack (DFP) for CCES
How to create a new project for the ADuCM3029
How to add startup code and core components to a new project for the ADuCM3029
How to import existing projects into your workspace
How to build projects for programming the ADuCM3029
How to configure the Tools Settings used by an ADuCM3029 project
How to configure the debug session for an ADuCM3029 application
How to start and stop debugging an ADuCM3029 application
How to create an Intel Hex (.hex) file from an ADuCM3029 application
Workspace and Projects
A CCES workspace is a folder (e.g. c:\Users\anon\cces\2.6.0) that contains project resources and metadata.
When projects are created or imported, details about that project are stored in the workspace. The workspace metadata also includes preferences set through the CCES Preferences dialog box and IDE window layouts.
By default, CCES creates new projects within your workspace folder.
Each time you start CCES, you will be prompted for a workspace location. You can opt to default to a workspace directory by choosing to use a workspace directory as your default. You will not be prompted the next time you open CCES.
How to install or upgrade the ADuCM302x Device Family Pack (DFP) for CCES
CCES 2.6.0 does not comes with the ADuCM302x Device Family Pack (DFP) and ARM CMSIS Pack file pre-installed.
To install the ADuCM302x DFP:
Switch to the CMSIS Pack Manager perspective by selecting Window | Perspective | Open Perspective | Other… | CMSIS Pack Manager.
Once opened, select Check for Updates on Web ( blue arrows on the toolbar ). This may time a minute or two.
Choose Analog Devices and ADuCM302x Series in the Devices View.
Select the ADuCM302x CMSIS Pack version (choose version 2.0.0 or higher) from the Packs View.
Click the Install Action.
Alternatively, the ADuCM3029 Device Family Pack (DFP) files can be installed using a local download.
After downloading the .pack files from the Keil website (https://www.keil.com/dd2/pack/), select the Import Packs button in the CMSIS Pack Manager's Packs View, choose the .pack file as shown in the screenshot below, and click Open.
You will be prompted to accept a license agreement and, after agreeing to it, the CMSIS-Pack file will be installed into CrossCore Embedded Studio's CMSIS-Pack installation directory (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices).
To install the ARM 4.5.0 CMSIS Pack:
Switch to the CMSIS Pack Manager perspective by selecting Window | Perspective | Open Perspective | Other… | CMSIS Pack Manager.
Once opened, select Check for Updates on Web ( blue arrows on the toolbar ), if you have not already done so.
Choose ARM in the Devices View.
Select the Generic and ARM.CMSIS from the Packs View, select version 4.5.0
Click the Install Action.
ADuCM302x Board Support Packs (BSP)
There are two Board Support Packs (BSP) available: one for the ADuCM302x EZ-Kit and one for the ADICUP3029. These BSPs can be installed in the same way as the Device Family Pack (DFP) via the CMSIS Pack Manager perspective.
ADuCM302x EZ-Kit Board Support Pack
The ADuCM302x EZ-Kit Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the ADuCM302x EZ-Kit and examples for all the peripherals in the ADuCM302x processor. The examples in the BSP depend on the drivers from ADuCM302x Device Family Pack (DFP). The BSP is designed to work with CrossCore Embedded Studio and Keil uVision.
For more information on the ADuCM302x EZ-Kit BSP, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADuCM302x_EZ_KIT_BSP\2.0.0\Documents\ADuCM302x_EZ-KIT_BSP_Users_Guide.pdf)
ADICUP3029 Board Support Pack
The ADICUP3029 Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the ADICUP3029 Evaluation Board and examples for peripherals on the ADUCM3029 processor. The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio and the ADuCM302x Device Family Pack (DFP).
For more information on the ADICUP3029 BSP, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\EVAL-ADICUP3029_BSP\1.0.0\Documents\EVAL-ADICUP3029_Users_Guide.pdf)
ADI Sensor Software Pack
The ADI Sensor Software pack contains various sensor software components and associated examples. The examples in the sensor pack are designed to work with ADICUP3029 board and associated sensor shields. ADI Sensor Software requires CrossCore Embedded Studio (CCES), ADuCM302x Device Family Pack (DFP) and ADICUP3029 Board Support Pack (BSP).
For more information on the ADI Sensor Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-SensorSoftware\1.0.0\Documents\SensorSoftware_Users_Guide.pdf)
How to create a new project for the ADuCM3029
A project for ADuCM3029 can be created using the New CrossCore Project Wizard. This wizard will guide you through the steps to create a new project.
To create a new project, go to the menu bar and find File → New → CrossCore Project.
Choose Processor family ARM and select Processor type ADuCM3029.
Choose your Silicon revision (default is 1.0).
A SILICON_REVISION macro will be set in your project's Tools Settings, allowing you to conditionally check the silicon revision in your source code.
Project configuration allows you to add additional Add-ins to your project, such as Pin Multiplexing and changing the template language for a generated main function etc.
Finally, press Finish and the project will be created and you can begin writing your program.
How to add startup code and core components to a new project for the ADuCM3029
An out-of-the-box ADuCM3029 project does not have startup code or a linker description file that maps code and data. It is necessary to add these components using the Run-time Environment (RTE) Configuration Editor.
CrossCore Projects created for Analog Devices' Cortex-M based processors, such as ADuCM3029 include a system.rteconfig file. Opening this file within the IDE will open the RTE Configuration Editor. Components from the CMSIS-Pack, such as drivers and services, can be added to a project by selecting them in the editor and clicking Save.
At minimum, a new ADuCM3029 project will require the Device::Startup, CMSIS::Core and Device::Global Configuration components to be added to the project.
Double-click on the system.rteconfig to open the RTE Configuration Editor.
Select Device::Startup, CMSIS::Core and Device::Global Configuration.
Click Save (Ctrl+S)
You can also choose Device::Startup and click the Resolve button to add dependant components
How to import existing projects into your workspace
There are three(3) methods for importing existing projects:
Examples that you have saved to a local drive on your PC.
Examples that come with the ADuCM3029 Device Family Pack (DFP).
Examples which are in the ADICUP3029 GIT repository (most up to date content).
How to Import Existing Projects Saved to a Local Drive
Select File | Import… from the CCES menu.
A dialog will pop-up with several importing options, choose the General | Existing Projects into Workspace option, and click Next
Select Browse in the dialog window and search for the saved project which is on your local drive.
(Optional) If the Copy projects into workspace option is checked, the project will be copied to your workspace folder and the newly copied project will be opened and used. This preserves the original version of the project.
Click Finish
How to Import Examples that come with the ADuCM3029 Device Family Pack (DFP) or Board Support Packs (BSP)
Examples are provided with the ADuCM3029 DFP and BSPs and can be opened from the CMSIS Pack Manager Perspective Examples View.
Open CMSIS Pack Manager perspective by clicking “Open Perspective” icon on tool bar and selecting “CMSIS Pack Manager” in the Open Perspective window (or choose CMSIS Pack Manager perspective if already open).
From the Examples View, select the example that you would like to open.
Click the Copy Action button.
A dialog will pop-up showing the location where the example will be copied to. Click Copy to copy and open the example project.
The CCES Examples Browser can also be used to open examples by Help | Browse Examples.
Select ADuCM302x_DFP[x.y.z] in Product drop-down list, select the example and click Open example. Then the example will be copied to your workspace.
How to Import Existing Projects from the GIT Repository
( Note that at the time of writing, the EVAL-ADICUP3029 GIT repo. is work In Progress )
Open the GIT perspective by clicking “Open Perspective” icon on tool bar and selecting “Git” in the Open Perspective window (or choose the GIT perspective if already open).
Clone the Git repository which contains all the latest code and projects associated with the ADuCM360. Populate the
URI field with the following address.
-
Click Next, Next and then Finish. There may be a pause while the branches are fetched.
In the Git Repositories window, Right Click on the Projects folder and select Import Projects…
Select Import existing Eclipse projects
Click Next and then Finish
How to build projects for programming the ADuCM3029
Open the C perspective by clicking “Open Perspective” icon on tool bar and selecting C in the Open Perspective window (or choose the C perspective if already open).
Right click on the project and select the Build Project.
Select the project in the Project Explorer View.
Select the Cog icon from the View's toolbar.
After configuring your project, click Apply and/or OK.
You will need to create a launch configuration to debug your ADuCM3029 program.
If you have already built a project, select that project in the Project Explorer View.
Right-click on the project and choose
Debug As and
Application with GDB and OpenOCD (Emulator)
In the Target tab, choose Target (processor) and in the drop-down select Analog Devices ADuCM3029
In the Target tab, choose Interface and in the drop-down select ARM CMSIS-DAP compliant adapter
In the Main tab, ensure that your project is selected in the Project entry box.
If the correct project is not populated, click the
Browse… button and choose the project. Note that this is optional and you only need to choose a project if you want the
IDE to search a project for the built binaries (programs), otherwise you can leave this entry blank.
In the Main tab, ensure your binary (program) is selected in the Application entry box.
If the correct binary (program) is not populated, click on Search Project… and choose the binary (program) from those available in the chosen project.
If your binary (program) is not populated and it was not built from a project in your workspace (
i.e. you have a pre-built binary), then click the
Browse… button and search for your pre-built binary (program). Click
Open when you have found and selected the pre-built binary (program).
Hardware breakpoints are limited in your ADuCM3029 application
When you click Debug or Apply, you will be prompted with a dialog informing your the Hardware Breakpoints are limited. Click Yes. You can opt to not show this dialog again.
How to start and stop debugging an ADuCM3029 application
Ensure that you have connected your EVAL-ADICUP3029 board to your computer via the
USB port (the micro
USB connected closest to the DC barrel jack).
If you are already in the Debug Configurations dialog, then click Debug.
If you are in the C Perspective, then you can launch the last Debug session by clicking the Beetle Debug button on the toolbar.
You will be prompted to switch perspective to the Debug perspective. Click Yes. You can opt to not show this dialog again.
If your binary (program) was built with semi-hosting enabled, then CCES will warn you that you need to re-build the program when you want to run the program without a debugger attached.
To disable semi-hosting in your program, visit your project Tools Settings.
Change the
semi-hosting support option under
Linker | Libraries to nosys.specs or None, depending on whether or not your program is currently using semi-hosting (
e.g. printf).
After configuring your project, click Apply and/or OK.
Right click on the project and select the Build Project.
If this is the first time you have launched OpenOCD, the Windows Firewall may pop-up a window asking for access. Click on “Allow Access”.
If everything goes fine, in the Console window, you will see a report without errors.
As a reference, the full text should be similar to:
Open On-Chip Debugger (OpenOCD) 0.9.0
Licensed under GNU GPL v2
Report bugs to <openocd-devel@lists.sourceforge.net>
0
Info : select transport "swd"
adapter speed: 1000 kHz
cortex_m reset_config sysresetreq
Info : CMSIS-DAP: SWD Supported
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : CMSIS-DAP: FW Version = 1.0
Info : SWCLK/TCK = 0 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 1000 kHz
Info : SWD IDCODE 0x2ba01477
Info : aducm3029.cpu: hardware has 2 breakpoints, 1 watchpoints
Info : CHIPID 0x0284
memory bus access delay set to 6 tck
adapter speed: 1000 kHz
Info : accepting 'gdb' connection on tcp/3333
Your program's execution is stopped automatically at the first breakpoint which is at the beginning of main() loop. You can use the debug functions and features of the CCES environment. (Such as stepping through, breakpoints, register reads, variable values, etc.)
To terminate a debug session, click on the red Stop button on the toolbar.
How to create an Intel Hex (.hex) file from an ADuCM3029 application
Ensure that your program is built with semi-hosting disabled by visiting Tools Settings | Linker | Libraries and change Semihosting support to nosys.specs or None, depending on your application set-up.
Rebuild your application.
Convert your application into Intel Hex (.hex) format by visiting Tools Settings once more.
Select the Build Steps tab.
Add the following command to the
Post-build steps | Command entry box:
arm-none-eabi-objcopy -O ihex ${ProjName} ${ProjName}.hex
Rebuild your application.
End of Document