This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:tools:cces_user_guide [10 Oct 2017 21:08] – updating to the second release, added videos, and edited flow Brandon Bushey | resources:eval:user-guides:eval-adicup3029:tools:cces_user_guide [03 Mar 2018 09:39] – [Workspace and Projects] Andrew McLachlan | ||
---|---|---|---|
Line 22: | Line 22: | ||
- How to start and stop debugging an ADuCM3029 application | - How to start and stop debugging an ADuCM3029 application | ||
- How to create an Intel Hex (.hex) file from an ADuCM3029 application | - How to create an Intel Hex (.hex) file from an ADuCM3029 application | ||
+ | |||
+ | <WRAP center round info 60%> | ||
+ | We have a playlist of **YOUTUBE VIDEOS** that can help you understand different functions and features of CrossCore Embedded Studio. [[https:// | ||
+ | </ | ||
===== Workspace and Projects ===== | ===== Workspace and Projects ===== | ||
- | A CCES workspace is a folder (e.g. c: | + | A CCES workspace is a folder (e.g. c: |
When projects are created or imported, details about that project are stored in the workspace. The workspace metadata also includes preferences set through the CCES Preferences dialog box and IDE window layouts. | When projects are created or imported, details about that project are stored in the workspace. The workspace metadata also includes preferences set through the CCES Preferences dialog box and IDE window layouts. | ||
By default, CCES creates new projects within your workspace folder. | By default, CCES creates new projects within your workspace folder. | ||
Line 207: | Line 211: | ||
\\ | \\ | ||
- | - To disable semi-hosting in your program, visit your project Tools Settings. | + | - To enable/disable semi-hosting in your program, visit your project |
- | - Change the // | + | - Change the // |
+ | * Enable semi-hosting by selecting the **rdimon.specs** option. | ||
+ | * Use this option if using the debugger for things like printf() or other similar tools. | ||
+ | * Disable | ||
+ | * Use this option for standalone embedded operation. | ||
- After configuring your project, click Apply and/or OK. | - After configuring your project, click Apply and/or OK. | ||
- Right click on the project and select the //Build Project//. | - Right click on the project and select the //Build Project//. |