This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:eval-adicup3029:tools:cces_setup_guide [03 Jan 2021 21:55] Robin Getz fix links |
resources:eval:user-guides:eval-adicup3029:tools:cces_setup_guide [09 Nov 2022 15:29] Brandon Bushey [CrossCore Embedded Studio Download Packages] redirecting to Crosscore web page instead of older versions of CrossCore |
||
---|---|---|---|
Line 31: | Line 31: | ||
<WRAP round 100% download> | <WRAP round 100% download> | ||
- | The EVAL-ADICUP3029 **requires** the use of {{http://analog.com/cces | Crosscore Embedded Studios}} version **2.6.0 or higher**. Do not attempt to use earlier versions of the CrossCore tools, due to compatibility issues that will **damage** the EVAL-ADICUP3029.\\ | + | The EVAL-ADICUP3029 **requires** the use of Crosscore Embedded Studios version **2.6.0 or higher**. Do not attempt to use earlier versions of the CrossCore tools, due to compatibility issues that will **damage** the EVAL-ADICUP3029.\\ |
\\ | \\ | ||
- | {{http://download.analog.com/tools/CrossCoreEmbeddedStudio/Releases/Release_2.8.0/ADI_CrossCoreEmbeddedStudio-Rel2.8.0.exe | CrossCore Embedded Studio 2.8.0 Windows Installer(Executable)}} | + | [[adi>en/design-center/evaluation-hardware-and-software/software/adswt-cces.html| CrossCore Embedded Studio for Windows and Linux]] |
- | + | ||
- | {{http://download.analog.com/tools/CrossCoreEmbeddedStudio/Releases/Release_2.8.0/adi-CrossCoreEmbeddedStudio-linux-x86-2.8.0.deb | CrossCore Embedded Studio 2.8.0 Ubuntu Linux Installer(Debian)}} | + | |
</WRAP> | </WRAP> |