Wiki

This version (20 Jan 2022 22:35) was approved by Brandon Bushey.The Previously approved version (30 Jul 2019 20:08) is available.Diff

Wi-Fi Software Pack

This CMSIS pack and its contents are DEPRECATED and no longer supported. Please do not use this moving forward

General Description/Overview

Wi-Fi software pack contains source code written to interface the ADuCM3029 with the ESP8266 Wi-Fi radio module.(Found on the EVAL-ADICUP3029) This software package acts as a library that can be used with any platform containing the ADuCM3029 and the ESP8266.

To use the ADI_WifiSoftware Pack with the ADICUP3029, you will also require the following software, tools, CMSIS Packs:

  • CrossCore Embedded Studio
  • ADuCM302x Device Family Pack
  • ADICUP3029 Board Support Package

For detailed information regarding the WiFi software pack, please see our complete WiFi software user guide.

You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications using the WiFi for the ADICUP3029 platform.

Downloading the WiFi Software Pack

The software pack can be downloaded in several ways.

  1. Downloaded via the tools program
    • It is recommended to download the WiFi software pack through from the tools program you are using. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the WiFi software pack through CrossCore Embedded Studio please see our CrossCore Embedded Studio Quickstart User Guide.
  2. Downloaded to local directory
    • However if you do decide to download the WiFi software pack to your PC/laptop directly, please use the link below, and make sure you save the software pack to the correct local directory for your applications/projects.

Download the WiFi Software Pack to your computer.

Wi-Fi Software Pack 1.0.1

End of Document

resources/eval/user-guides/eval-adicup3029/software/wifi_sw.txt · Last modified: 20 Jan 2022 22:35 by Brandon Bushey