The ADICUP3029 platform is built upon a software framework that has many layers. In order to run any of the examples shown with this platform, it is extremely important that all users have the following software packs installed in their tools.
The simplified diagram below describes the interaction between all packs and the applications, and how the packs are built on top of each other. In order to import, create, or debug applications with the ADICUP3029, it is important to ensure all packs are installed before running an example.