This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:smart_greenhouse [23 Apr 2021 17:47] – Removing Arrow Connect Brandon Bushey | resources:eval:user-guides:eval-adicup3029:reference_designs:smart_greenhouse [18 Aug 2021 16:54] – [Demo Requirements] Brandon Bushey | ||
---|---|---|---|
Line 169: | Line 169: | ||
* EVAL-CN0398-ARDZ | * EVAL-CN0398-ARDZ | ||
* EVAL-CN0410-ARDZ | * EVAL-CN0410-ARDZ | ||
- | * ESP8266 Module | ||
- | * Internet connected gateway – utilize existing Wi-Fi gateway/ | ||
* Cables/ | * Cables/ | ||
Line 177: | Line 175: | ||
* Sensors/ | * Sensors/ | ||
- | * An LED light bar | + | * An LED light bar (We used the [[ADI> |
- | * A pH probe | + | * A pH probe (We used the [[http:// |
- | * A moisture sensor | + | * A moisture sensor |
- | * A PT100 RTD | + | * A PT100 RTD (Any 3-wire PT100 should work) |
* Software | * Software | ||
Line 195: | Line 193: | ||
- Configure CS jumper for **CN0397** to pins **3** and **4**.{{: | - Configure CS jumper for **CN0397** to pins **3** and **4**.{{: | ||
- Configure CS jumper on **P21** for **CN0410** to pins **1** and **2**. An external power supply must be used to power the board and the jumper on **P20** must be set to **1** and **2**.{{: | - Configure CS jumper on **P21** for **CN0410** to pins **1** and **2**. An external power supply must be used to power the board and the jumper on **P20** must be set to **1** and **2**.{{: | ||
- | - The Led Bar must be connected to the CN0410 board to enable power to the leds. Also to select the leds we want to controll | + | - The Led Bar must be connected to the CN0410 board to enable power to the leds. Also to select the leds we want to control |
==== Serial Terminal Smart Greenhouse Source Code ==== | ==== Serial Terminal Smart Greenhouse Source Code ==== | ||
Line 227: | Line 225: | ||
The greenhouse application involves 3 layers: | The greenhouse application involves 3 layers: | ||
- | * Hardware, | + | * Hardware, |
* Communication layer (SPI communication) | * Communication layer (SPI communication) | ||
* Processing layer (ADICUP3029 and ESP8266) | * Processing layer (ADICUP3029 and ESP8266) | ||
Line 257: | Line 255: | ||
For more detailed instructions on importing this application/ | For more detailed instructions on importing this application/ | ||
- | |||
- | |||
// End of Document // | // End of Document // | ||
- | |||
- |