This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0503 [06 Oct 2020 09:48] – [Obtaining the Source Code] - add hex file Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0503 [20 Sep 2022 15:25] (current) – [Hardware User Guide and Demo Guides] adding nitrate demo link Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Optical Platform Demo (w/ EVAL-CN0503-ADRZ) ====== | + | ====== Optical Platform |
The **ADuCM3029_demo_cn0503** project provides a solution to get multiple liquid parameters (for example turbidity, pH, fluorescence, | The **ADuCM3029_demo_cn0503** project provides a solution to get multiple liquid parameters (for example turbidity, pH, fluorescence, | ||
Line 86: | Line 86: | ||
| | //FL_READ CMD// | Read a specific device or application parameter value from the software buffer.\\ //cmd// = register or application command to input the relevant parameter.\\ For register commands the buffer contains an array of register-value pairs that will be written in order to the device. Calling this function with a regiter command will display the value of the first occurrence of the register.\\ The only application command supported by this command is the def command. Calling the DEF command will read that value from the software buffer. | FL_READ REG? 10A - return the first value of the register 0x10A\\ FL_READ DEF2? RFLT - display the setting of the ration 2 filter bandwidth from the software buffer. | | | | //FL_READ CMD// | Read a specific device or application parameter value from the software buffer.\\ //cmd// = register or application command to input the relevant parameter.\\ For register commands the buffer contains an array of register-value pairs that will be written in order to the device. Calling this function with a regiter command will display the value of the first occurrence of the register.\\ The only application command supported by this command is the def command. Calling the DEF command will read that value from the software buffer. | FL_READ REG? 10A - return the first value of the register 0x10A\\ FL_READ DEF2? RFLT - display the setting of the ration 2 filter bandwidth from the software buffer. | | ||
- | ===== Obtaining the Source Code ===== | + | ===== Obtaining the Software |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code, include files, and executable file (.HEX) of the **ADuCM3029_demo_cn0503** can be found here: | + | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing |
- | <WRAP round 80% download> | + | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download |
- | [[https:// | + | The software for the **ADuCM3029_demo_cn0503** can be found here: |
- | {{ :resources: | + | <WRAP round 80% download> |
+ | Prebuilt CN0503 Hex File | ||
+ | * [[https:// | ||
+ | Complete CN0503 Source Files | ||
+ | * [[https://github.com/ | ||
</ | </ | ||
Line 132: | Line 138: | ||
- Use example scripts from [[https:// | - Use example scripts from [[https:// | ||
+ | ===== Hardware User Guide and Demo Guides ===== | ||
+ | |||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[: | ||
// End of Document // | // End of Document // |