Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0503 [21 Apr 2020 12:18]
AndreiD1994 remove tmplate notice
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0503 [07 Jul 2020 11:57] (current)
AndreiD1994 [Setting up the Hardware]
Line 36: Line 36:
  
   - Set up the the **EVAL-CN0503-ARDZ** as shown in the [[resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503#​assembling_the_mechanical_fixtures | Hardware User Guide]].   - Set up the the **EVAL-CN0503-ARDZ** as shown in the [[resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503#​assembling_the_mechanical_fixtures | Hardware User Guide]].
-  - Connect the board to the **EVAL-ADICUP3029** via the Arduino headers. ​FIXME add picture +  - Connect the board to the **EVAL-ADICUP3029** via the Arduino headers. ​{{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​cn0503_arduino.jpg |}} 
-  - Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. ​FIXME add picture+  - Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. ​{{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​cn0503_system_pc.jpg |}}
  
 ===== Configuring the Software ===== ===== Configuring the Software =====
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0503.txt · Last modified: 07 Jul 2020 11:57 by AndreiD1994