Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0418 [24 May 2019 09:08]
AndreiD1994 Update link to source code
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0418 [12 Jun 2019 13:22] (current)
AndreiD1994 [Setting up the Hardware]
Line 35: Line 35:
  
   - Connect **EVAL-CN0418-ARDZ** to the **EVAL-ADICUP3029**.   - Connect **EVAL-CN0418-ARDZ** to the **EVAL-ADICUP3029**.
-  - Set the jumpers into the position shown below. This is the standard position and only works for one board systems. ​FIXME picture+  - Set the jumpers into the position shown below. This is the standard position and only works for one board systems. ​{{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​cn0418_jumper_position.jpg |}}
   - Connect a micro-USB cable to **P10** connector of the **EVAL-ADICUP3029** and connect it to a computer.   - Connect a micro-USB cable to **P10** connector of the **EVAL-ADICUP3029** and connect it to a computer.
-  - Connect the 24V power source to the **P1** connector with the ground wire to pin 2 and 24V wire to pin 3. The final setup should look similar to the picture below. ​FIXME picture.+  - Connect the 24V power source to the **P1** connector with the ground wire to pin 2 and 24V wire to pin 3. The final setup should look similar to the picture below. ​{{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​cn0418_final_hw_setup.jpg |}}
  
 ===== Configuring the Software ===== ===== Configuring the Software =====
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0418.txt · Last modified: 12 Jun 2019 13:22 by AndreiD1994