Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0415 [27 Feb 2019 07:54]
AndreiD1994 Embedd terminal setup page
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0415 [27 Feb 2019 08:00] (current)
AndreiD1994 Update pictures
Line 66: Line 66:
 ===== Setting up the Hardware ===== ===== Setting up the Hardware =====
  
-  - Connect **EVAL-CN0415-ARDZ** board to the **EVAL-ADICUP3029**. {{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​cn0415_stacked_adicup3029.jpg?​nolink ​| CN0415 ​stacked ​on ADICUP3029}}+  - Connect **EVAL-CN0415-ARDZ** board to the **EVAL-ADICUP3029**. {{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​cn0415_adicup3029_dock.jpeg | CN0415 ​docked ​on ADICUP3029 }}
   - Connect a micro-USB cable to **P10** connector of the **EVAL-ADICUP3029** and connect it to a computer.   - Connect a micro-USB cable to **P10** connector of the **EVAL-ADICUP3029** and connect it to a computer.
   - Connect a solenoid actuator to the **P8** connector with the positive wire on pin 1 and negative wire on pin 2.   - Connect a solenoid actuator to the **P8** connector with the positive wire on pin 1 and negative wire on pin 2.
-  - Connect a 12V power supply to the **P1** connector with the positive wire on pin 1 and negative wire on pin 2.{{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​powered_cn0415.jpg?​nolink ​Powered ​CN0415 ​board with solenoid}}+  - Connect a 12V power supply to the **P1** connector with the positive wire on pin 1 and negative wire on pin 2.{{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​cn0415_fully_connected.jpeg | CN0415 ​power up }}
   - Turn on power supply.   - Turn on power supply.
 ===== Configuring the Software ===== ===== Configuring the Software =====
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0415.txt · Last modified: 27 Feb 2019 08:00 by AndreiD1994