This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0414 [12 Feb 2019 14:38] – Correct application name Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0414 [03 Mar 2021 02:55] (current) – [Obtaining the Source Code] adding in .Hex files Brandon Bushey | ||
---|---|---|---|
Line 57: | Line 57: | ||
===== Outputting Data ===== | ===== Outputting Data ===== | ||
- | ==== Serial Terminal Output ==== | + | {{page>/ |
- | + | ||
- | The program outputs data and **CLI** interface to a serial terminal through **UART**. | + | |
- | + | ||
- | - In order to view the data, you must flash the program to the EVAL-ADICUP3029. | + | |
- | - Then follow the UART settings below with the serial terminal program. | + | |
- | + | ||
- | Following is the UART configuration. | + | |
- | Select COM Port | + | |
- | Baud rate: 115200 | + | |
- | Data: 8 bit | + | |
- | Parity: none | + | |
- | Stop: 1 bit | + | |
- | Flow Control: none | + | |
- | \\ | + | |
- | The terminal program must interpret new line as **LF** and **local echo** must be enabled. | + | |
==== Available commands ==== | ==== Available commands ==== | ||
Line 111: | Line 96: | ||
- | ===== Obtaining the Source Code ===== | + | ===== Obtaining the Software |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the **ADuCM3029_demo_cn0414** can be found here: | + | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. |
+ | |||
+ | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | ||
+ | |||
+ | The software for the **ADuCM3029_demo_cn0414** can be found here: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | + | Prebuilt CN0414 Hex File | |
- | [[https:// | + | * [[https:// |
+ | Complete CN0414 Source Files | ||
+ | * [[https:// | ||
</ | </ | ||
- | |||
- | |||
===== How to use the Tools ===== | ===== How to use the Tools ===== | ||